ADC_Init_TypeDef Struct ReferenceEMLIB > ADC
ADC initialization structure, common for single conversion and scan sequence.
Definition at line
781
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
| ADC_LPFilter_TypeDef | lpfMode |
| ADC_OvsRateSel_TypeDef | ovsRateSel |
| uint8_t | prescale |
| bool | tailgate |
| uint8_t | timebase |
| ADC_Warmup_TypeDef | warmUpMode |
Field Documentation
| ADC_LPFilter_TypeDef ADC_Init_TypeDef::lpfMode |
Lowpass or decoupling capacitor filter.
Definition at line
790
of file
em_adc.h
.
Referenced by ADC_Init() .
| ADC_OvsRateSel_TypeDef ADC_Init_TypeDef::ovsRateSel |
Oversampling rate select. To have any effect, oversampling must be enabled for single/scan mode.
Definition at line
786
of file
em_adc.h
.
Referenced by ADC_Init() , and TOUCH_Init() .
| uint8_t ADC_Init_TypeDef::prescale |
Clock division factor N, ADC clock = HFPERCLK / (N + 1).
Definition at line
806
of file
em_adc.h
.
Referenced by ADC_Init() , adcInit() , MIC_init() , and TOUCH_Init() .
| bool ADC_Init_TypeDef::tailgate |
Enable/disable conversion tailgating.
Definition at line
809
of file
em_adc.h
.
Referenced by ADC_Init() .
| uint8_t ADC_Init_TypeDef::timebase |
Timebase for ADC warm up. Select N to give (N+1)HFPERCLK cycles. (Additional delay is added for bandgap references. See the reference manual for more information.) Normally, N should be selected so that the timebase is at least 1 us. See ADC_TimebaseCalc() to obtain a suggested timebase of, at least, 1 us.
Definition at line
803
of file
em_adc.h
.
Referenced by ADC_Init() , adcInit() , and MIC_init() .
| ADC_Warmup_TypeDef ADC_Init_TypeDef::warmUpMode |
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_adc.h