VCMP_TypeDef Struct ReferenceDevices > EFM32LG_VCMP
Definition at line
48
of file
efm32lg_vcmp.h
.
Data Fields |
|
| __IOM uint32_t | CTRL |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | INPUTSEL |
| __IM uint32_t | STATUS |
Field Documentation
| __IOM uint32_t VCMP_TypeDef::CTRL |
Control Register
Definition at line
49
of file
efm32lg_vcmp.h
.
| __IOM uint32_t VCMP_TypeDef::IEN |
Interrupt Enable Register
Definition at line
52
of file
efm32lg_vcmp.h
.
| __IM uint32_t VCMP_TypeDef::IF |
Interrupt Flag Register
Definition at line
53
of file
efm32lg_vcmp.h
.
| __IOM uint32_t VCMP_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
55
of file
efm32lg_vcmp.h
.
| __IOM uint32_t VCMP_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
54
of file
efm32lg_vcmp.h
.
| __IOM uint32_t VCMP_TypeDef::INPUTSEL |
Input Selection Register
Definition at line
50
of file
efm32lg_vcmp.h
.
| __IM uint32_t VCMP_TypeDef::STATUS |
Status Register
Definition at line
51
of file
efm32lg_vcmp.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/
efm32lg_vcmp.h