PRS_TypeDef Struct ReferenceDevices > EFM32LG_PRS

Definition at line 48 of file efm32lg_prs.h .

Data Fields

PRS_CH_TypeDef CH [12]
uint32_t RESERVED0 [1]
__IOM uint32_t ROUTE
__IOM uint32_t SWLEVEL
__IOM uint32_t SWPULSE

Field Documentation

PRS_CH_TypeDef PRS_TypeDef::CH[12]

Channel registers

Definition at line 54 of file efm32lg_prs.h .

uint32_t PRS_TypeDef::RESERVED0[1]

Reserved registers

Definition at line 53 of file efm32lg_prs.h .

__IOM uint32_t PRS_TypeDef::ROUTE

I/O Routing Register

Definition at line 51 of file efm32lg_prs.h .

__IOM uint32_t PRS_TypeDef::SWLEVEL

Software Level Register

Definition at line 50 of file efm32lg_prs.h .

__IOM uint32_t PRS_TypeDef::SWPULSE

Software Pulse Register

Definition at line 49 of file efm32lg_prs.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32LG/Include/ efm32lg_prs.h