USB_EndpointDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON

USB Endpoint Descriptor.

Definition at line 490 of file em_usb.h.

#include <em_usb.h>

Data Fields

uint8_t bDescriptorType
 
uint8_t bEndpointAddress
 
uint8_t bInterval
 
uint8_t bLength
 
uint8_t bmAttributes
 
uint16_t wMaxPacketSize
 

Field Documentation

uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType

Constant ENDPOINT Descriptor Type

Definition at line 492 of file em_usb.h.

Referenced by USBH_PrintEndpointDescriptor().

uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress

The address of the endpoint

Definition at line 493 of file em_usb.h.

Referenced by USBD_Init(), USBH_AssignHostChannel(), and USBH_PrintEndpointDescriptor().

uint8_t USB_EndpointDescriptor_TypeDef::bInterval

Interval for polling EP for data transfers

Definition at line 496 of file em_usb.h.

Referenced by USBH_PrintEndpointDescriptor(), USBH_Read(), and USBH_Write().

uint8_t USB_EndpointDescriptor_TypeDef::bLength

Size of this descriptor in bytes

Definition at line 491 of file em_usb.h.

Referenced by USBH_PrintEndpointDescriptor().

uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes

This field describes the endpoint attributes

Definition at line 494 of file em_usb.h.

Referenced by USBD_Init(), USBH_AssignHostChannel(), and USBH_PrintEndpointDescriptor().

uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize

Maximum packet size for the endpoint

Definition at line 495 of file em_usb.h.

Referenced by USBD_Init(), USBH_AssignHostChannel(), and USBH_PrintEndpointDescriptor().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/em_usb.h