ADC_InitScanInput_TypeDef Struct ReferenceEMLIB > ADC
Scan input configuration.
Definition at line
850
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
| uint32_t | scanInputEn |
| uint32_t | scanInputSel |
| uint32_t | scanNegSel |
Field Documentation
| uint32_t ADC_InitScanInput_TypeDef::scanInputEn |
Input enable mask.
Definition at line
855
of file
em_adc.h
.
| uint32_t ADC_InitScanInput_TypeDef::scanInputSel |
Input range select to be applied to ADC_SCANINPUTSEL.
Definition at line
852
of file
em_adc.h
.
| uint32_t ADC_InitScanInput_TypeDef::scanNegSel |
Alternative negative input.
Definition at line
858
of file
em_adc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_adc.h