BURTC_Init_TypeDef Struct ReferenceEMLIB > BURTC
BURTC initialization structure.
Definition at line
112
of file
em_burtc.h
.
#include <
em_burtc.h
>
Data Fields |
|
uint32_t | clkDiv |
BURTC_ClkSel_TypeDef | clkSel |
bool | compare0Top |
bool | debugRun |
bool | enable |
uint32_t | lowPowerComp |
BURTC_LP_TypeDef | lowPowerMode |
BURTC_Mode_TypeDef | mode |
bool | timeStamp |
Field Documentation
uint32_t BURTC_Init_TypeDef::clkDiv |
Clock divider; for ULFRCO 1Khz or 2kHz operation.
Definition at line
118
of file
em_burtc.h
.
Referenced by BURTC_Init() .
BURTC_ClkSel_TypeDef BURTC_Init_TypeDef::clkSel |
bool BURTC_Init_TypeDef::compare0Top |
Set if Compare Value 0 is also top value (counter restart).
Definition at line
123
of file
em_burtc.h
.
Referenced by BURTC_Init() .
bool BURTC_Init_TypeDef::debugRun |
If true, counter will keep running under debug halt.
Definition at line
116
of file
em_burtc.h
.
Referenced by BURTC_Init() .
bool BURTC_Init_TypeDef::enable |
Enable BURTC after initialization (starts counter).
Definition at line
113
of file
em_burtc.h
.
Referenced by BURTC_Init() .
uint32_t BURTC_Init_TypeDef::lowPowerComp |
Number of least significantt clock bits to ignore in low power mode.
Definition at line
120
of file
em_burtc.h
.
Referenced by BURTC_Init() .
BURTC_LP_TypeDef BURTC_Init_TypeDef::lowPowerMode |
Low power operation mode, requires LFXO or LFRCO.
Definition at line
125
of file
em_burtc.h
.
Referenced by BURTC_Init() .
BURTC_Mode_TypeDef BURTC_Init_TypeDef::mode |
Configure energy mode operation.
Definition at line
115
of file
em_burtc.h
.
Referenced by BURTC_Init() .
bool BURTC_Init_TypeDef::timeStamp |
Enable time stamp on entering backup power domain.
Definition at line
121
of file
em_burtc.h
.
Referenced by BURTC_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_burtc.h