CdcKit Drivers
Detailed Description
Implements USB Communication Device Class (CDC).
CDC implementation.
The source code of the CDC implementation resides in kits/common/drivers/cdc.c and cdc.h . This driver implements a basic USB to RS232 bridge.
CDC device configuration options.
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file. The values shown below are from the Giant Gecko DK3750 CDC example.
// USB interface numbers. Interfaces are numbered from zero to one less than
// the number of concurrent interfaces supported by the configuration. A CDC
// device is by itself a composite device and has two interfaces.
// The interface numbers must be 0 and 1 for a standalone CDC device, for a
// composite device which includes a CDC interface it must not be in conflict
// with other device interfaces.
#define CDC_CTRL_INTERFACE_NO ( 0 )
#define CDC_DATA_INTERFACE_NO ( 1 )
// Endpoint address for CDC data reception.
#define CDC_EP_DATA_OUT ( 0x01 )
// Endpoint address for CDC data transmission.
#define CDC_EP_DATA_IN ( 0x81 )
// Endpoint address for the notification endpoint (not used).
#define CDC_EP_NOTIFY ( 0x82 )
// Timer id, see USBTIMER in the USB device stack documentation.
// The CDC driver has a Rx timeout functionality which require a timer.
#define CDC_TIMER_ID ( 0 )
// DMA related macros, select DMA channels and DMA request signals.
#define CDC_UART_TX_DMA_CHANNEL ( 0 )
#define CDC_UART_RX_DMA_CHANNEL ( 1 )
#define CDC_TX_DMA_SIGNAL DMAREQ_UART1_TXBL
#define CDC_RX_DMA_SIGNAL DMAREQ_UART1_RXDATAV
// UART/USART selection macros.
#define CDC_UART UART1
#define CDC_UART_CLOCK cmuClock_UART1
#define CDC_UART_ROUTE ( UART_ROUTE_RXPEN | UART_ROUTE_TXPEN | \
UART_ROUTE_LOCATION_LOC2 )
#define CDC_UART_TX_PORT gpioPortB
#define CDC_UART_TX_PIN 9
#define CDC_UART_RX_PORT gpioPortB
#define CDC_UART_RX_PIN 10
// Activate the RS232 switch on DK's.
#define CDC_ENABLE_DK_UART_SWITCH() BSP_PeripheralAccess(BSP_RS232_UART, true)
// No RS232 switch on STK's. Leave the definition "empty".
#define CDC_ENABLE_DK_UART_SWITCH()
Functions |
|
| void | CDC_Init (void) |
|
CDC device initialization.
|
|
| int | CDC_SetupCmd (const USB_Setup_TypeDef *setup) |
|
Handle USB setup commands. Implements CDC class specific commands.
|
|
| void | CDC_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
|
Callback function called each time the USB device state is changed. Starts CDC operation when device has been configured by USB host.
|
|
Function Documentation
| int CDC_SetupCmd | ( | const USB_Setup_TypeDef * |
setup
|
) |
Handle USB setup commands. Implements CDC class specific commands.
- Parameters
-
[in] setupPointer to the setup packet received.
- Returns
- USB_STATUS_OK if command accepted. USB_STATUS_REQ_UNHANDLED when command is unknown, the USB device stack will handle the request.
Definition at line
183
of file
cdc.c
.
| void CDC_StateChangeEvent | ( | USBD_State_TypeDef |
oldState,
|
| USBD_State_TypeDef |
newState
|
||
| ) |
Callback function called each time the USB device state is changed. Starts CDC operation when device has been configured by USB host.
- Parameters
-
[in] oldStateThe device state the device has just left. [in] newStateThe new device state.
Definition at line
236
of file
cdc.c
.