MSDSCSI_ReadCapacity_TypeDef Struct ReferenceKit Drivers > Msd

SCSI Read Capacity Command Descriptor Block (CDB) typedef.

Definition at line 175 of file msdscsi.h .

#include < msdscsi.h >

Data Fields

struct {
uint8_t Obsolete : 1
uint8_t Reserved1 : 7
};
struct {
uint8_t Pmi : 1
uint8_t Reserved3 : 7
};
uint8_t Control
uint32_t Lba
uint8_t OpCode
uint16_t Reserved2

Field Documentation

uint8_t MSDSCSI_ReadCapacity_TypeDef::Control

Control byte.

Definition at line 187 of file msdscsi.h .

uint32_t MSDSCSI_ReadCapacity_TypeDef::Lba

Logical Block (sector) Address.

Definition at line 181 of file msdscsi.h .

uint8_t MSDSCSI_ReadCapacity_TypeDef::Obsolete

Obsolete, expect any value.

Definition at line 178 of file msdscsi.h .

uint8_t MSDSCSI_ReadCapacity_TypeDef::OpCode

Command opcode.

Definition at line 176 of file msdscsi.h .

uint8_t MSDSCSI_ReadCapacity_TypeDef::Pmi

Partial medium indicator.

Definition at line 184 of file msdscsi.h .

uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved1

Reserved, expect 0.

Definition at line 179 of file msdscsi.h .

uint16_t MSDSCSI_ReadCapacity_TypeDef::Reserved2

Reserved, expect 0.

Definition at line 182 of file msdscsi.h .

uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved3

Reserved, expect 0.

Definition at line 185 of file msdscsi.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/ msdscsi.h