Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Receive plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
| struct | EZRADIODRV_PacketRxHandle |
|
EzRadio receive plug-in instance initialization and handler structure.
|
|
Macros |
|
| #define | EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT |
|
Configuration data for EzRadio receive plug-in.
|
|
Typedefs |
|
| typedef struct EZRADIODRV_PacketRxHandle | EZRADIODRV_PacketRxHandle_t |
|
EzRadio receive plug-in instance initialization and handler structure.
|
|
Functions |
|
| Ecode_t | ezradioStartRx ( EZRADIODRV_Handle_t radioHandle) |
|
Set Radio to RX mode, packet length is always coming from the radio configuration.
|
|
Macro Definition Documentation
| #define EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio receive plug-in.
Definition at line
74
of file
ezradio_receive_plugin.h
.
Function Documentation
| Ecode_t ezradioStartRx | ( | EZRADIODRV_Handle_t |
radioHandle
|
) |
Set Radio to RX mode, packet length is always coming from the radio configuration.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where packet buffer, callback and channel configurations are set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
64
of file
ezradio_receive_plugin.c
.
References EZRADIODRV_PacketRxHandle::channel , ECODE_EMDRV_EZRADIODRV_OK , ezradio_start_rx() , and EZRADIODRV_HandleData::packetRx .