ecode.h File Reference

Energy Aware drivers error code definitions.

Version
5.5.0

License

(C) Copyright 2015 Silicon Labs, www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file ecode.h.

#include <stdint.h>

Macros

#define ECODE_EMDRV_BASE   (0xF0000000U)
 Base value for all EMDRV errorcodes.
 
#define ECODE_EMDRV_DMADRV_BASE   (ECODE_EMDRV_BASE | 0x00008000U)
 Base value for DMADRV error codes.
 
#define ECODE_EMDRV_EZRADIODRV_BASE   (ECODE_EMDRV_BASE | 0x00009000U)
 Base value for EZRADIODRV error codes.
 
#define ECODE_EMDRV_NVM3_BASE   (ECODE_EMDRV_BASE | 0x0000E000U)
 Base value for NVM3 error codes.
 
#define ECODE_EMDRV_NVM_BASE   (ECODE_EMDRV_BASE | 0x00003000U)
 Base value for NVM error codes.
 
#define ECODE_EMDRV_RTCDRV_BASE   (ECODE_EMDRV_BASE | 0x00001000U)
 Base value for RTCDRV error codes.
 
#define ECODE_EMDRV_SPIDRV_BASE   (ECODE_EMDRV_BASE | 0x00002000U)
 Base value for SPIDRV error codes.
 
#define ECODE_EMDRV_TEMPDRV_BASE   (ECODE_EMDRV_BASE | 0x0000D000U)
 Base value for TEMPDRV error codes.
 
#define ECODE_EMDRV_UARTDRV_BASE   (ECODE_EMDRV_BASE | 0x00007000U)
 Base value for UARTDRV error codes.
 
#define ECODE_EMDRV_USTIMER_BASE   (ECODE_EMDRV_BASE | 0x00004000U)
 Base value for USTIMER error codes.
 
#define ECODE_OK   (0U)
 Generic success return value.
 

Typedefs

typedef uint32_t Ecode_t
 Typedef for API function error code return values.