RMU_TypeDef Struct ReferenceDevices > RMU
RMU Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_rmu.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_rmu.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | RST | 
| __IM uint32_t | RSTCAUSE | 
Field Documentation
| __IOM uint32_t RMU_TypeDef::CMD | 
Command Register
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_rmu.h
        
        .
       
| __IOM uint32_t RMU_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_rmu.h
        
        .
       
| __IOM uint32_t RMU_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_rmu.h
        
        .
       
| __IOM uint32_t RMU_TypeDef::RST | 
Reset Control Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_rmu.h
        
        .
       
| __IM uint32_t RMU_TypeDef::RSTCAUSE | 
Reset Cause Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_rmu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       efr32bg14p_rmu.h