LESENSE_TypeDef Struct ReferenceDevices > LESENSE
LESENSE Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_lesense.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_lesense.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | ALTEXCONF | 
| __IOM uint32_t | BIASCTRL | 
| LESENSE_BUF_TypeDef | BUF [16] | 
| __IM uint32_t | BUFDATA | 
| LESENSE_CH_TypeDef | CH [16] | 
| __IOM uint32_t | CHEN | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IM uint32_t | CURCH | 
| __IOM uint32_t | DECCTRL | 
| __IOM uint32_t | DECSTATE | 
| __IOM uint32_t | EVALCTRL | 
| __IOM uint32_t | IDLECONF | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | PERCTRL | 
| __IOM uint32_t | PRSCTRL | 
| __IM uint32_t | PTR | 
| uint32_t | RESERVED0 [2] | 
| uint32_t | RESERVED1 [38] | 
| __IOM uint32_t | ROUTEPEN | 
| __IOM uint32_t | SCANRES | 
| __IOM uint32_t | SENSORSTATE | 
| LESENSE_ST_TypeDef | ST [32] | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IOM uint32_t | TIMCTRL | 
Field Documentation
| __IOM uint32_t LESENSE_TypeDef::ALTEXCONF | 
Alternative Excite Pin Configuration
        Definition at line
        
         67
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::BIASCTRL | 
Bias Control Register
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| LESENSE_BUF_TypeDef LESENSE_TypeDef::BUF[16] | 
Scanresult
        Definition at line
        
         79
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IM uint32_t LESENSE_TypeDef::BUFDATA | 
Result Buffer Data Register
        Definition at line
        
         62
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| LESENSE_CH_TypeDef LESENSE_TypeDef::CH[16] | 
Scanconfig
        Definition at line
        
         81
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::CHEN | 
Channel Enable Register
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::CMD | 
Command Register
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IM uint32_t LESENSE_TypeDef::CURCH | 
Current Channel Index
        Definition at line
        
         63
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::DECCTRL | 
Decoder Control Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::DECSTATE | 
Current Decoder State
        Definition at line
        
         64
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::EVALCTRL | 
LESENSE Evaluation Control
        Definition at line
        
         55
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::IDLECONF | 
GPIO Idle Phase Configuration
        Definition at line
        
         66
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         72
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IM uint32_t LESENSE_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         69
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         71
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         70
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::PERCTRL | 
Peripheral Control Register
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::PRSCTRL | 
PRS Control Register
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IM uint32_t LESENSE_TypeDef::PTR | 
Result Buffer Pointers
        Definition at line
        
         61
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| uint32_t LESENSE_TypeDef::RESERVED0[2] | 
Reserved for future use
        Definition at line
        
         68
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| uint32_t LESENSE_TypeDef::RESERVED1[38] | 
Reserved registers
        Definition at line
        
         76
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::ROUTEPEN | 
I/O Routing Register
        Definition at line
        
         74
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::SCANRES | 
Scan Result Register
        Definition at line
        
         59
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::SENSORSTATE | 
Decoder Input Register
        Definition at line
        
         65
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| LESENSE_ST_TypeDef LESENSE_TypeDef::ST[32] | 
Decoding states
        Definition at line
        
         77
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IM uint32_t LESENSE_TypeDef::STATUS | 
Status Register
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IM uint32_t LESENSE_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         73
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
| __IOM uint32_t LESENSE_TypeDef::TIMCTRL | 
Timing Control Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_lesense.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       efr32bg14p_lesense.h