HAL_LayerEMDRV > EZRADIODRV
Detailed Description
EzRadio HAL Layer
.
Functions |
|
void | ezradio_hal_AssertShutdown (void) |
void | ezradio_hal_ClearNsel (void) |
void | ezradio_hal_DeassertShutdown (void) |
void | ezradio_hal_GpioInit ( GPIOINT_IrqCallbackPtr_t ezradioIrqCallback, bool enablePTI) |
uint8_t | ezradio_hal_NirqLevel (void) |
void | ezradio_hal_SetNsel (void) |
void | ezradio_hal_SpiInit (void) |
void | ezradio_hal_SpiReadByte (uint8_t *readByte) |
void | ezradio_hal_SpiReadData (uint8_t byteCount, uint8_t *pData) |
void | ezradio_hal_SpiWriteByte (uint8_t byteToWrite) |
void | ezradio_hal_SpiWriteData (uint8_t byteCount, uint8_t *pData) |
void | ezradio_hal_SpiWriteReadData (uint8_t byteCount, uint8_t *txData, uint8_t *rxData) |
Function Documentation
void ezradio_hal_AssertShutdown | ( | void |
|
) |
Asserts SDN pin of the EZRadio device.
Definition at line
137
of file
ezradio_hal.c
.
References GPIO_PinOutSet() .
Referenced by ezradio_reset() .
void ezradio_hal_ClearNsel | ( | void |
|
) |
Clears nSEL pin of the EZRadio device.
Definition at line
153
of file
ezradio_hal.c
.
References GPIO_PinOutClear() .
Referenced by ezradio_comm_GetResp() , ezradio_comm_ReadData() , ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
void ezradio_hal_DeassertShutdown | ( | void |
|
) |
Deasserts SDN pin of the EZRadio device.
Definition at line
145
of file
ezradio_hal.c
.
References GPIO_PinOutClear() .
Referenced by ezradio_reset() .
void ezradio_hal_GpioInit | ( | GPIOINT_IrqCallbackPtr_t |
ezradioIrqCallback,
|
bool |
enablePTI
|
||
) |
Configures the EZRadio GPIO port and pins
- Parameters
-
[in] ezradioIrqCallback
EZRadio interrupt callback configuration [in] enablePTI
If true enables the radio PTI bridge in the controller.
Definition at line
66
of file
ezradio_hal.c
.
References CMU_ClockEnable() , cmuClock_PRS , GPIO_InputSenseSet() , GPIO_IntConfig() , GPIO_PinModeSet() , GPIOINT_CallbackRegister() , gpioModeInput , gpioModeInputPull , gpioModePushPull , PRS , PRS_CH_CTRL_SIGSEL_GPIOPIN14 , PRS_CH_CTRL_SIGSEL_GPIOPIN15 , PRS_CH_CTRL_SOURCESEL_GPIOH , and PRS_SourceAsyncSignalSet() .
Referenced by ezradioInit() .
uint8_t ezradio_hal_NirqLevel | ( | void |
|
) |
Reads nIRQ pin of the EZRadio device.
- Returns
- Value of nIRQ pin.
Definition at line
171
of file
ezradio_hal.c
.
References GPIO_PinInGet() .
Referenced by ezradio_configuration_init() .
void ezradio_hal_SetNsel | ( | void |
|
) |
Sets nSEL pin of the EZRadio device.
Definition at line
161
of file
ezradio_hal.c
.
References GPIO_PinOutSet() .
Referenced by ezradio_comm_GetResp() , ezradio_comm_ReadData() , ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
void ezradio_hal_SpiInit | ( | void |
|
) |
Initializes SPI driver for the EZRadio device.
Definition at line
123
of file
ezradio_hal.c
.
References SPIDRV_Init::bitRate , SPIDRV_Init::csControl , SPIDRV_Init() , and spidrvCsControlApplication .
Referenced by ezradioInit() .
void ezradio_hal_SpiReadByte | ( | uint8_t * |
readByte
|
) |
Reads a single byte from the EZRadio SPI port.
- Parameters
-
readByte
Read byte.
Definition at line
203
of file
ezradio_hal.c
.
References SPIDRV_MReceiveB() .
Referenced by ezradio_comm_GetResp() .
void ezradio_hal_SpiReadData | ( | uint8_t |
byteCount,
|
uint8_t * |
pData
|
||
) |
Reads byteCount number of bytes from the EZRadio SPI port.
- Parameters
-
byteCount
Number of bytes to write. pData
Pointer to the byte array.
Definition at line
225
of file
ezradio_hal.c
.
References SPIDRV_MReceiveB() .
Referenced by ezradio_comm_GetResp() , and ezradio_comm_ReadData() .
void ezradio_hal_SpiWriteByte | ( | uint8_t |
byteToWrite
|
) |
Writes a single byte to the EZRadio SPI port.
- Parameters
-
byteToWrite
Byte to write.
Definition at line
193
of file
ezradio_hal.c
.
References SPIDRV_MTransmitB() .
Referenced by ezradio_comm_GetResp() , ezradio_comm_ReadData() , and ezradio_comm_WriteData() .
void ezradio_hal_SpiWriteData | ( | uint8_t |
byteCount,
|
uint8_t * |
pData
|
||
) |
Writes byteCount number of bytes to the EZRadio SPI port.
- Parameters
-
byteCount
Number of bytes to write. pData
Pointer to the byte array.
Definition at line
214
of file
ezradio_hal.c
.
References SPIDRV_MTransmitB() .
Referenced by ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
void ezradio_hal_SpiWriteReadData | ( | uint8_t |
byteCount,
|
uint8_t * |
txData,
|
||
uint8_t * |
rxData
|
||
) |
Reads byteCount number of bytes from the EZRadio SPI port.
- Parameters
-
byteCount
Number of bytes to write. pData
Pointer to the byte array.
Definition at line
236
of file
ezradio_hal.c
.
References SPIDRV_MTransferB() .
Referenced by ezradio_comm_GetResp() , and ezradio_comm_ReadData() .