LETIMER_TypeDef Struct ReferenceDevices > LETIMER
LETIMER Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_letimer.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_letimer.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CNT | 
| __IOM uint32_t | COMP0 | 
| __IOM uint32_t | COMP1 | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | PRSSEL | 
| __IOM uint32_t | REP0 | 
| __IOM uint32_t | REP1 | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [2] | 
| uint32_t | RESERVED2 [2] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IOM uint32_t | ROUTEPEN | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
Field Documentation
| __IOM uint32_t LETIMER_TypeDef::CMD | 
Command Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_Enable() , LETIMER_Init() , and LETIMER_Reset() .
| __IOM uint32_t LETIMER_TypeDef::CNT | 
Counter Value Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_CounterGet() .
| __IOM uint32_t LETIMER_TypeDef::COMP0 | 
Compare Value Register 0
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_CompareGet() , LETIMER_CompareSet() , and LETIMER_Reset() .
| __IOM uint32_t LETIMER_TypeDef::COMP1 | 
Compare Value Register 1
        Definition at line
        
         55
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_CompareGet() , LETIMER_CompareSet() , and LETIMER_Reset() .
| __IOM uint32_t LETIMER_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_Init() , and LETIMER_Reset() .
| __IOM uint32_t LETIMER_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         61
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_IntDisable() , LETIMER_IntEnable() , LETIMER_IntGetEnabled() , and LETIMER_Reset() .
| __IM uint32_t LETIMER_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_IntGet() , and LETIMER_IntGetEnabled() .
| __IOM uint32_t LETIMER_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_IntClear() , and LETIMER_Reset() .
| __IOM uint32_t LETIMER_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         59
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_IntSet() .
| __IOM uint32_t LETIMER_TypeDef::PRSSEL | 
PRS Input Select Register
        Definition at line
        
         71
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
| __IOM uint32_t LETIMER_TypeDef::REP0 | 
Repeat Counter Register 0
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_RepeatGet() , LETIMER_RepeatSet() , and LETIMER_Reset() .
| __IOM uint32_t LETIMER_TypeDef::REP1 | 
Repeat Counter Register 1
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
Referenced by LETIMER_RepeatGet() , LETIMER_RepeatSet() , and LETIMER_Reset() .
| uint32_t LETIMER_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         63
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
| uint32_t LETIMER_TypeDef::RESERVED1[2] | 
Reserved for future use
        Definition at line
        
         66
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
| uint32_t LETIMER_TypeDef::RESERVED2[2] | 
Reserved for future use
        Definition at line
        
         70
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
| __IOM uint32_t LETIMER_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         68
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
| __IOM uint32_t LETIMER_TypeDef::ROUTEPEN | 
I/O Routing Pin Enable Register
        Definition at line
        
         67
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
| __IM uint32_t LETIMER_TypeDef::STATUS | 
| __IM uint32_t LETIMER_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         64
        
        of file
        
         efr32bg14p_letimer.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       efr32bg14p_letimer.h