VDAC_TypeDef Struct ReferenceDevices > VDAC
VDAC Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_vdac.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_vdac.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CAL | 
| __IOM uint32_t | CH0CTRL | 
| __IOM uint32_t | CH0DATA | 
| __IOM uint32_t | CH1CTRL | 
| __IOM uint32_t | CH1DATA | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | COMBDATA | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| VDAC_OPA_TypeDef | OPA [2] | 
| uint32_t | RESERVED0 [27] | 
| __IM uint32_t | STATUS | 
Field Documentation
| __IOM uint32_t VDAC_TypeDef::CAL | 
Calibration Register
        Definition at line
        
         62
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_Init() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::CH0CTRL | 
Channel 0 Control Register
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_InitChannel() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::CH0DATA | 
Channel 0 Data Register
        Definition at line
        
         59
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_Channel0OutputSet() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::CH1CTRL | 
Channel 1 Control Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_InitChannel() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::CH1DATA | 
Channel 1 Data Register
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_Channel1OutputSet() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::CMD | 
Command Register
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_Enable() , VDAC_Init() , VDAC_InitChannel() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::COMBDATA | 
Combined Data Register
        Definition at line
        
         61
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
| __IOM uint32_t VDAC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_Init() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_IntDisable() , VDAC_IntEnable() , VDAC_IntGetEnabled() , and VDAC_Reset() .
| __IM uint32_t VDAC_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         55
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_IntGet() , and VDAC_IntGetEnabled() .
| __IOM uint32_t VDAC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_IntClear() , and VDAC_Reset() .
| __IOM uint32_t VDAC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_IntSet() .
| VDAC_OPA_TypeDef VDAC_TypeDef::OPA[2] | 
OPA Registers
        Definition at line
        
         65
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
| uint32_t VDAC_TypeDef::RESERVED0[27] | 
Reserved registers
        Definition at line
        
         64
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
| __IM uint32_t VDAC_TypeDef::STATUS | 
Status Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_vdac.h
        
        .
       
Referenced by VDAC_Enable() , VDAC_Init() , VDAC_InitChannel() , and VDAC_Reset() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       efr32bg14p_vdac.h