SMU_TypeDef Struct ReferenceDevices > SMU
SMU Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_smu.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_smu.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | PPUCTRL | 
| __IM uint32_t | PPUFS | 
| __IOM uint32_t | PPUPATD0 | 
| __IOM uint32_t | PPUPATD1 | 
| uint32_t | RESERVED0 [3] | 
| uint32_t | RESERVED1 [9] | 
| uint32_t | RESERVED2 [3] | 
| uint32_t | RESERVED3 [14] | 
Field Documentation
| __IOM uint32_t SMU_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IM uint32_t SMU_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IOM uint32_t SMU_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IOM uint32_t SMU_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IOM uint32_t SMU_TypeDef::PPUCTRL | 
PPU Control Register
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IM uint32_t SMU_TypeDef::PPUFS | 
PPU Fault Status
        Definition at line
        
         63
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IOM uint32_t SMU_TypeDef::PPUPATD0 | 
PPU Privilege Access Type Descriptor 0
        Definition at line
        
         59
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| __IOM uint32_t SMU_TypeDef::PPUPATD1 | 
PPU Privilege Access Type Descriptor 1
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| uint32_t SMU_TypeDef::RESERVED0[3] | 
Reserved for future use
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| uint32_t SMU_TypeDef::RESERVED1[9] | 
Reserved for future use
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| uint32_t SMU_TypeDef::RESERVED2[3] | 
Reserved for future use
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
| uint32_t SMU_TypeDef::RESERVED3[14] | 
Reserved for future use
        Definition at line
        
         62
        
        of file
        
         efr32bg14p_smu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       efr32bg14p_smu.h