MSC_TypeDef Struct ReferenceDevices > MSC
MSC Register Declaration
Definition at line
49
of file
efr32bg14p_msc.h
.
#include <
efr32bg14p_msc.h
>
Data Fields |
|
| __IOM uint32_t | AAPUNLOCKCMD |
| __IOM uint32_t | ADDRB |
| __IOM uint32_t | BOOTLOADERCTRL |
| __IOM uint32_t | CACHECMD |
| __IOM uint32_t | CACHECONFIG0 |
| __IM uint32_t | CACHEHITS |
| __IM uint32_t | CACHEMISSES |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | LOCK |
| __IOM uint32_t | MASSLOCK |
| __IOM uint32_t | READCTRL |
| uint32_t | RESERVED0 [1] |
| uint32_t | RESERVED1 [4] |
| uint32_t | RESERVED2 [1] |
| uint32_t | RESERVED3 [1] |
| uint32_t | RESERVED4 [5] |
| uint32_t | RESERVED5 [6] |
| __IOM uint32_t | STARTUP |
| __IM uint32_t | STATUS |
| __IOM uint32_t | WDATA |
| __IOM uint32_t | WRITECMD |
| __IOM uint32_t | WRITECTRL |
Field Documentation
| __IOM uint32_t MSC_TypeDef::AAPUNLOCKCMD |
Software Unlock AAP Command Register
Definition at line
80
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::ADDRB |
Page Erase/Write Address Buffer
Definition at line
54
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::BOOTLOADERCTRL |
Bootloader Read and Write Enable, Write Once Register
Definition at line
79
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::CACHECMD |
Flash Cache Command Register
Definition at line
65
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::CACHECONFIG0 |
Cache Configuration Register 0
Definition at line
81
of file
efr32bg14p_msc.h
.
| __IM uint32_t MSC_TypeDef::CACHEHITS |
Cache Hits Performance Counter
Definition at line
66
of file
efr32bg14p_msc.h
.
| __IM uint32_t MSC_TypeDef::CACHEMISSES |
Cache Misses Performance Counter
Definition at line
67
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::CMD |
Command Register
Definition at line
76
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::CTRL |
Memory System Control Register
Definition at line
50
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::IEN |
Interrupt Enable Register
Definition at line
63
of file
efr32bg14p_msc.h
.
| __IM uint32_t MSC_TypeDef::IF |
Interrupt Flag Register
Definition at line
60
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
62
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
61
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::LOCK |
Configuration Lock Register
Definition at line
64
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::MASSLOCK |
Mass Erase Lock Register
Definition at line
70
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::READCTRL |
Read Control Register
Definition at line
51
of file
efr32bg14p_msc.h
.
| uint32_t MSC_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line
55
of file
efr32bg14p_msc.h
.
| uint32_t MSC_TypeDef::RESERVED1[4] |
Reserved for future use
Definition at line
59
of file
efr32bg14p_msc.h
.
| uint32_t MSC_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line
69
of file
efr32bg14p_msc.h
.
| uint32_t MSC_TypeDef::RESERVED3[1] |
Reserved for future use
Definition at line
72
of file
efr32bg14p_msc.h
.
| uint32_t MSC_TypeDef::RESERVED4[5] |
Reserved for future use
Definition at line
75
of file
efr32bg14p_msc.h
.
| uint32_t MSC_TypeDef::RESERVED5[6] |
Reserved for future use
Definition at line
78
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::STARTUP |
Startup Control
Definition at line
73
of file
efr32bg14p_msc.h
.
| __IM uint32_t MSC_TypeDef::STATUS |
Status Register
Definition at line
57
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::WDATA |
Write Data Register
Definition at line
56
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::WRITECMD |
Write Command Register
Definition at line
53
of file
efr32bg14p_msc.h
.
| __IOM uint32_t MSC_TypeDef::WRITECTRL |
Write Control Register
Definition at line
52
of file
efr32bg14p_msc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
efr32bg14p_msc.h