EepromKit Drivers
| Macros | |
| #define | EEPROM_DVK_ADDR 0xA0 | 
| Functions | |
| int | EEPROM_Read ( I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) | 
| Read data from EEPROM. | |
| int | EEPROM_Write ( I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) | 
| Write data to EEPROM. | |
Macro Definition Documentation
| #define EEPROM_DVK_ADDR 0xA0 | 
I2C device address for EEPROM on DK
        Definition at line
        
         40
        
        of file
        
         eeprom.h
        
        .
       
Function Documentation
| int EEPROM_Read | ( | I2C_TypeDef * | 
            i2c,
            | 
| uint8_t | 
            addr,
            | ||
| unsigned int | 
            offset,
            | ||
| uint8_t * | 
            data,
            | ||
| unsigned int | 
            len
            | ||
| ) | 
Read data from EEPROM.
- Parameters
- 
         [in] i2cPointer to I2C peripheral register block. [in] addrI2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit. [in] offsetOffset in EEPROM to start reading from. [out] dataLocation to place read data, must be at least lenlong.[in] lenNumber of bytes to read. 
- Returns
- Returns number of bytes read. Less than specified number of bytes is returned if reading beyond end of EEPROM. Negative value is returned is some sort of error occurred during read.
        Definition at line
        
         118
        
        of file
        
         eeprom.c
        
        .
       
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , EEPROM_DVK_LEN , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_READ , I2CSPM_Transfer() , i2cTransferDone , and I2C_TransferSeq_TypeDef::len .
| int EEPROM_Write | ( | I2C_TypeDef * | 
            i2c,
            | 
| uint8_t | 
            addr,
            | ||
| unsigned int | 
            offset,
            | ||
| uint8_t * | 
            data,
            | ||
| unsigned int | 
            len
            | ||
| ) | 
Write data to EEPROM.
- Parameters
- 
         [in] i2cPointer to I2C peripheral register block. [in] addrI2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit. [in] offsetOffset in EEPROM to start writing to. [out] dataLocation holding data to write, must be at least lenlong.[in] lenNumber of bytes to write. 
- Returns
- Returns number of bytes written. Less than specified number of bytes is returned if writing beyond end of EEPROM. Negative value is returned is some sort of error occurred during write.
        Definition at line
        
         179
        
        of file
        
         eeprom.c
        
        .
       
References I2C_TransferSeq_TypeDef::addr , I2C_TransferSeq_TypeDef::buf , I2C_TransferSeq_TypeDef::data , EEPROM_AckPoll() , EEPROM_DVK_LEN , EEPROM_DVK_PAGESIZE , I2C_TransferSeq_TypeDef::flags , I2C_FLAG_WRITE_WRITE , I2CSPM_Transfer() , i2cTransferDone , and I2C_TransferSeq_TypeDef::len .