TRNG_TypeDef Struct ReferenceDevices > TRNG
TRNG Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg14p_trng.h
       
       .
      
      
       #include <
       
     
        efr32bg14p_trng.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CONTROL | 
| __IM uint32_t | FIFO | 
| __IM uint32_t | FIFODEPTH | 
| __IM uint32_t | FIFOLEVEL | 
| __IOM uint32_t | INITWAITVAL | 
| __IOM uint32_t | KEY0 | 
| __IOM uint32_t | KEY1 | 
| __IOM uint32_t | KEY2 | 
| __IOM uint32_t | KEY3 | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [3] | 
| uint32_t | RESERVED2 [50] | 
| __IOM uint32_t | STATUS | 
| __IOM uint32_t | TESTDATA | 
Field Documentation
| __IOM uint32_t TRNG_TypeDef::CONTROL | 
Main Control Register
        Definition at line
        
         50
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IM uint32_t TRNG_TypeDef::FIFO | 
FIFO Data
        Definition at line
        
         64
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IM uint32_t TRNG_TypeDef::FIFODEPTH | 
FIFO Depth Register
        Definition at line
        
         53
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IM uint32_t TRNG_TypeDef::FIFOLEVEL | 
FIFO Level Register
        Definition at line
        
         51
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::INITWAITVAL | 
Initial Wait Counter
        Definition at line
        
         62
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::KEY0 | 
Key Register 0
        Definition at line
        
         54
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::KEY1 | 
Key Register 1
        Definition at line
        
         55
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::KEY2 | 
Key Register 2
        Definition at line
        
         56
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::KEY3 | 
Key Register 3
        Definition at line
        
         57
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| uint32_t TRNG_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         52
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| uint32_t TRNG_TypeDef::RESERVED1[3] | 
Reserved for future use
        Definition at line
        
         60
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| uint32_t TRNG_TypeDef::RESERVED2[50] | 
Reserved for future use
        Definition at line
        
         63
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::STATUS | 
Status Register
        Definition at line
        
         61
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
| __IOM uint32_t TRNG_TypeDef::TESTDATA | 
Test Data Register
        Definition at line
        
         58
        
        of file
        
         efr32bg14p_trng.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG14P/Include/
       efr32bg14p_trng.h