ustimer.c File Reference
Microsecond delay functions.
- Version
- 5.5.0
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        ustimer.c
       
       .
      
       #include <stdbool.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_common.h
       
       "
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        em_emu.h
       
       "
      
      
       #include "
       
        em_core.h
       
       "
      
      
       #include "
       
        em_timer.h
       
       "
      
      
       #include "
       
        ustimer.h
       
       "
      
      
| Functions | |
| Ecode_t | USTIMER_DeInit (void) | 
| Deinitialize USTIMER driver. | |
| Ecode_t | USTIMER_Delay (uint32_t usec) | 
| Delay a given number of microseconds. | |
| Ecode_t | USTIMER_DelayIntSafe (uint32_t usec) | 
| Delay a given number of microseconds. | |
| Ecode_t | USTIMER_Init (void) | 
| Activate and initialize the hardware timer used to pace the 1 microsecond delay functions. | |