EM_TypeDef Struct Reference
Defines segment COM and BIT fields for Energy Modes on display.
Definition at line 82
of file segmentlcd.c
.
Data Fields | |
uint8_t | bit [5] |
uint8_t | com [5] |
Field Documentation
uint8_t EM_TypeDef::bit[5] |
uint8_t EM_TypeDef::com[5] |
LCD COM line (for multiplexing)
Definition at line 83
of file segmentlcd.c
.
Referenced by SegmentLCD_EnergyMode().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
segmentlcd.c