hidkbd.c File Reference
USB Human Interface Devices (HID) class keyboard driver.
- Version
- 5.6.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        hidkbd.c
       
       .
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_common.h
       
       "
      
      
       #include "
       
        em_usb.h
       
       "
      
      
       #include "
       
        hidkbd.h
       
       "
      
      
| Macros | |
| #define | DEFAULT_IDLE_RATE 500 | 
| Functions | |
| void | HIDKBD_Init ( HIDKBD_Init_t *init) | 
| Initialize HID Keyboard driver. | |
| void | HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report) | 
| Report a keyboard press/release event. | |
| int | HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup) | 
| Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command. | |
| void | HIDKBD_StateChangeEvent ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| Handle USB state change events, this function must be called each time the USB device state is changed. | |
| const char HIDKBD_ReportDescriptor[69] | SL_ATTRIBUTE_ALIGN (4) | 
Macro Definition Documentation
| #define DEFAULT_IDLE_RATE 500 | 
Default idle-rate recommended in the USB HID class specification.
        Definition at line
        
         61
        
        of file
        
         hidkbd.c
        
        .
       
Referenced by HIDKBD_StateChangeEvent() .
Function Documentation
| const char HIDKBD_ReportDescriptor [69] SL_ATTRIBUTE_ALIGN | ( | 4 | 
            | ) | 
HID report descriptor created with usb.org's "HID Descriptor Tool(DT)" version 2.4. The descriptor defines an input report which matches the HIDKBD_KeyReport_t typedef, and an output report with 3 bits for controlling NumLock, CapsLock and ScrollLock keyboard LED's