msdbot.c File Reference
Implements the host side of the Bulk Only Transport protocol for USB Mass Storage class Devices.
- Version
- 5.6.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        msdbot.c
       
       .
      
       #include "
       
        em_usb.h
       
       "
      
      
       #include "
       
        msdbot.h
       
       "
      
      
| Functions | |
| int | MSDBOT_Init (USBH_Ep_TypeDef *out, USBH_Ep_TypeDef *in) | 
| MSDBOT module initialization. | |
| int | MSDBOT_Xfer (void *cbw, void *data) | 
| Perform an MSD Bulk Only Transfer (BOT). | |
Function Documentation
| int MSDBOT_Init | ( | USBH_Ep_TypeDef * | 
            out,
            | 
| USBH_Ep_TypeDef * | 
            in
            | ||
| ) | 
MSDBOT module initialization.
- Parameters
- 
         [in] outPointer to an MSD bulk OUT endpoint structure. [in] inPointer to an MSD bulk IN endpoint structure. 
- Returns
- MSDBOT_STATUS_OK on success, else MSDBOT_INIT_ERROR .
        Definition at line
        
         57
        
        of file
        
         msdbot.c
        
        .
       
References MSDBOT_INIT_ERROR , MSDBOT_STATUS_OK , and PORT_FULL_SPEED .
Referenced by MSDSCSI_Init() .
| int MSDBOT_Xfer | ( | void * | 
            cbw,
            | 
| void * | 
            data
            | ||
| ) | 
Perform an MSD Bulk Only Transfer (BOT).
- Parameters
- 
         [in] cbwPointer to a Command Block Wrapper (CBW) data structure. [in] dataData buffer for data to be transferred. 
- Returns
- 
         A positive (or zero) value indicating the number of bytes transferred.
         
 A negative value indicates a transfer error code enumerated in MSDBOT_Status_TypeDef .
        Definition at line
        
         97
        
        of file
        
         msdbot.c
        
        .
       
References MSDBOT_CSW_TypeDef::bCSWStatus , MSDBOT_CBW_TypeDef::dCBWDataTransferLength , MSDBOT_CBW_TypeDef::Direction , MSDBOT_CMD_FAILED , MSDBOT_XFER_ERROR , USB_CLASS_MSD_CSW_CMDPASSED , and USB_STATUS_EP_STALLED .
Referenced by MSDSCSI_Inquiry() , MSDSCSI_Read10() , MSDSCSI_ReadCapacity() , MSDSCSI_RequestSense() , MSDSCSI_TestUnitReady() , and MSDSCSI_Write10() .