tftamapped.c File Reference
EFM32GG_DK3750, TFT Initialization and setup for Adress Mapped mode.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file tftamapped.c
.
#include <stdbool.h>
#include "em_device.h
"
#include "em_gpio.h
"
#include "em_ebi.h
"
#include "bsp.h
"
#include "tftamapped.h
"
#include "dmd/ssd2119/dmd_ssd2119.h"
#include "glib/glib.h
"
Functions | |
bool | TFT_AddressMappedInit (void) |
TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI) | |
Variables | |
static bool | runOnce = true |
Variable Documentation
|
static |
Flag to indicate that we need to initialize once if starting up in
Definition at line 27
of file tftamapped.c
.
Referenced by TFT_AddressMappedInit().