LETIMEREMLIB

Detailed Description

Low Energy Timer (LETIMER) Peripheral API.

This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.

Data Structures

struct LETIMER_Init_TypeDef

Macros

#define LETIMER_INIT_DEFAULT

Enumerations

enum LETIMER_RepeatMode_TypeDef {
letimerRepeatFree = _LETIMER_CTRL_REPMODE_FREE,
letimerRepeatOneshot = _LETIMER_CTRL_REPMODE_ONESHOT,
letimerRepeatBuffered = _LETIMER_CTRL_REPMODE_BUFFERED,
letimerRepeatDouble = _LETIMER_CTRL_REPMODE_DOUBLE
}
enum LETIMER_UFOA_TypeDef {
letimerUFOANone = _LETIMER_CTRL_UFOA0_NONE,
letimerUFOAToggle = _LETIMER_CTRL_UFOA0_TOGGLE,
letimerUFOAPulse = _LETIMER_CTRL_UFOA0_PULSE,
letimerUFOAPwm = _LETIMER_CTRL_UFOA0_PWM
}

Functions

uint32_t LETIMER_CompareGet ( LETIMER_TypeDef *letimer, unsigned int comp)
Get the LETIMER compare register value.
void LETIMER_CompareSet ( LETIMER_TypeDef *letimer, unsigned int comp, uint32_t value)
Set the LETIMER compare register value.
__STATIC_INLINE uint32_t LETIMER_CounterGet ( LETIMER_TypeDef *letimer)
Get LETIMER counter value.
void LETIMER_Enable ( LETIMER_TypeDef *letimer, bool enable)
Start/stop LETIMER.
void LETIMER_Init ( LETIMER_TypeDef *letimer, const LETIMER_Init_TypeDef *init)
Initialize LETIMER.
__STATIC_INLINE void LETIMER_IntClear ( LETIMER_TypeDef *letimer, uint32_t flags)
Clear one or more pending LETIMER interrupts.
__STATIC_INLINE void LETIMER_IntDisable ( LETIMER_TypeDef *letimer, uint32_t flags)
Disable one or more LETIMER interrupts.
__STATIC_INLINE void LETIMER_IntEnable ( LETIMER_TypeDef *letimer, uint32_t flags)
Enable one or more LETIMER interrupts.
__STATIC_INLINE uint32_t LETIMER_IntGet ( LETIMER_TypeDef *letimer)
Get pending LETIMER interrupt flags.
__STATIC_INLINE uint32_t LETIMER_IntGetEnabled ( LETIMER_TypeDef *letimer)
Get enabled and pending LETIMER interrupt flags.
__STATIC_INLINE void LETIMER_IntSet ( LETIMER_TypeDef *letimer, uint32_t flags)
Set one or more pending LETIMER interrupts from SW.
uint32_t LETIMER_RepeatGet ( LETIMER_TypeDef *letimer, unsigned int rep)
Get the LETIMER repeat register value.
void LETIMER_RepeatSet ( LETIMER_TypeDef *letimer, unsigned int rep, uint32_t value)
Set the LETIMER repeat counter register value.
void LETIMER_Reset ( LETIMER_TypeDef *letimer)
Reset LETIMER to the same state that it was in after a hardware reset.
void LETIMER_SyncWait ( LETIMER_TypeDef *letimer)
Wait for the LETIMER to complete all synchronization of register changes and commands.
__STATIC_INLINE uint32_t LETIMER_TopGet ( LETIMER_TypeDef *letimer)
Get the current LETIMER top value.
void LETIMER_TopSet ( LETIMER_TypeDef *letimer, uint32_t value)
Set the LETIMER top value.

Macro Definition Documentation

#define LETIMER_INIT_DEFAULT
Value:
{ \
true, /* Enable timer when initialization completes. */ \
false, /* Stop counter during debug halt. */ \
false, /* Do not load COMP0 into CNT on underflow. */ \
false, /* Do not load COMP1 into COMP0 when REP0 reaches 0. */ \
0, /* Idle value 0 for output 0. */ \
0, /* Idle value 0 for output 1. */ \
letimerUFOANone, /* No action on underflow on output 0. */ \
letimerUFOANone, /* No action on underflow on output 1. */ \
letimerRepeatFree, /* Count until stopped by SW. */ \
0 /* Use default top Value. */ \
}

Default configuration for LETIMER initialization structure.

Definition at line 127 of file em_letimer.h .

Referenced by MIC_init() .

Enumeration Type Documentation

Repeat mode.

Enumerator
letimerRepeatFree

Count until stopped by SW.

letimerRepeatOneshot

Count REP0 times.

letimerRepeatBuffered

Count REP0 times, if REP1 has been written to, it is loaded into REP0 when REP0 is about to be decremented to 0.

letimerRepeatDouble

Run as long as both REP0 and REP1 are not 0. Both REP0 and REP1 are decremented when counter underflows.

Definition at line 58 of file em_letimer.h .

Underflow action on output.

Enumerator
letimerUFOANone

No output action.

letimerUFOAToggle

Toggle output when counter underflows.

letimerUFOAPulse

Hold output one LETIMER clock cycle when counter underflows.

letimerUFOAPwm

Set output idle when counter underflows, and active when matching COMP1.

Definition at line 76 of file em_letimer.h .

Function Documentation

uint32_t LETIMER_CompareGet ( LETIMER_TypeDef * letimer,
unsigned int comp
)

Get the LETIMER compare register value.

Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] comp A compare register to get, either 0 or 1.
Returns
A compare register value, 0 if invalid register selected.

Definition at line 134 of file em_letimer.c .

References LETIMER_TypeDef::COMP0 , and LETIMER_TypeDef::COMP1 .

void LETIMER_CompareSet ( LETIMER_TypeDef * letimer,
unsigned int comp,
uint32_t value
)

Set the LETIMER compare register value.

Note
The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] comp A compare register to set, either 0 or 1.
[in] value An initialization value (<= 0x0000ffff).

Definition at line 179 of file em_letimer.c .

References _LETIMER_COMP0_COMP0_MASK , _LETIMER_COMP0_COMP0_SHIFT , LETIMER_TypeDef::COMP0 , and LETIMER_TypeDef::COMP1 .

Referenced by LETIMER_TopSet() , and MIC_init() .

__STATIC_INLINE uint32_t LETIMER_CounterGet ( LETIMER_TypeDef * letimer )

Get LETIMER counter value.

Parameters
[in] letimer Pointer to the LETIMER peripheral register block.
Returns
Current LETIMER counter value.

Definition at line 161 of file em_letimer.h .

References LETIMER_TypeDef::CNT .

void LETIMER_Enable ( LETIMER_TypeDef * letimer,
bool enable
)

Start/stop LETIMER.

Note
The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] enable True to enable counting, false to disable.

Definition at line 232 of file em_letimer.c .

References LETIMER_TypeDef::CMD , LETIMER_CMD_START , LETIMER_CMD_STOP , LETIMER_SYNCBUSY_CMD , and LETIMER_TypeDef::SYNCBUSY .

void LETIMER_Init ( LETIMER_TypeDef * letimer,
const LETIMER_Init_TypeDef * init
)

Initialize LETIMER.

Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet() . That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.

Note
The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] init A pointer to the LETIMER initialization structure.

Definition at line 326 of file em_letimer.c .

References _LETIMER_CTRL_REPMODE_SHIFT , _LETIMER_CTRL_UFOA0_SHIFT , _LETIMER_CTRL_UFOA1_SHIFT , LETIMER_Init_TypeDef::bufTop , LETIMER_TypeDef::CMD , LETIMER_TypeDef::COMP0 , LETIMER_Init_TypeDef::comp0Top , LETIMER_TypeDef::CTRL , LETIMER_Init_TypeDef::debugRun , LETIMER_Init_TypeDef::enable , LETIMER_CMD_START , LETIMER_CMD_STOP , LETIMER_CTRL_BUFTOP , LETIMER_CTRL_COMP0TOP , LETIMER_CTRL_DEBUGRUN , LETIMER_CTRL_OPOL0 , LETIMER_CTRL_OPOL1 , LETIMER_STATUS_RUNNING , LETIMER_SYNCBUSY_CMD , LETIMER_Init_TypeDef::out0Pol , LETIMER_Init_TypeDef::out1Pol , LETIMER_Init_TypeDef::repMode , LETIMER_TypeDef::STATUS , LETIMER_TypeDef::SYNCBUSY , LETIMER_Init_TypeDef::topValue , LETIMER_Init_TypeDef::ufoa0 , and LETIMER_Init_TypeDef::ufoa1 .

Referenced by MIC_init() .

__STATIC_INLINE void LETIMER_IntClear ( LETIMER_TypeDef * letimer,
uint32_t flags
)

Clear one or more pending LETIMER interrupts.

Parameters
[in] letimer Pointer to LETIMER peripheral register block.
[in] flags Pending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).

Definition at line 184 of file em_letimer.h .

References LETIMER_TypeDef::IFC .

Referenced by LETIMER_Reset() .

__STATIC_INLINE void LETIMER_IntDisable ( LETIMER_TypeDef * letimer,
uint32_t flags
)

Disable one or more LETIMER interrupts.

Parameters
[in] letimer Pointer to LETIMER peripheral register block.
[in] flags LETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).

Definition at line 204 of file em_letimer.h .

References LETIMER_TypeDef::IEN .

__STATIC_INLINE void LETIMER_IntEnable ( LETIMER_TypeDef * letimer,
uint32_t flags
)

Enable one or more LETIMER interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
Parameters
[in] letimer Pointer to the LETIMER peripheral register block.
[in] flags LETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).

Definition at line 225 of file em_letimer.h .

References LETIMER_TypeDef::IEN .

__STATIC_INLINE uint32_t LETIMER_IntGet ( LETIMER_TypeDef * letimer )

Get pending LETIMER interrupt flags.

Note
Event bits are not cleared by the use of this function.
Parameters
[in] letimer Pointer to LETIMER peripheral register block.
Returns
LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).

Definition at line 244 of file em_letimer.h .

References LETIMER_TypeDef::IF .

__STATIC_INLINE uint32_t LETIMER_IntGetEnabled ( LETIMER_TypeDef * letimer )

Get enabled and pending LETIMER interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Event bits are not cleared by the use of this function.
Parameters
[in] letimer Pointer to LETIMER peripheral register block.
Returns
Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
  • the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).

Definition at line 270 of file em_letimer.h .

References LETIMER_TypeDef::IEN , and LETIMER_TypeDef::IF .

__STATIC_INLINE void LETIMER_IntSet ( LETIMER_TypeDef * letimer,
uint32_t flags
)

Set one or more pending LETIMER interrupts from SW.

Parameters
[in] letimer Pointer to LETIMER peripheral register block.
[in] flags LETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).

Definition at line 293 of file em_letimer.h .

References LETIMER_TypeDef::IFS .

uint32_t LETIMER_RepeatGet ( LETIMER_TypeDef * letimer,
unsigned int rep
)

Get the LETIMER repeat register value.

Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] rep Repeat register to get, either 0 or 1.
Returns
Repeat register value, 0 if invalid register selected.

Definition at line 422 of file em_letimer.c .

References LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .

void LETIMER_RepeatSet ( LETIMER_TypeDef * letimer,
unsigned int rep,
uint32_t value
)

Set the LETIMER repeat counter register value.

Note
The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] rep Repeat counter register to set, either 0 or 1.
[in] value An initialization value (<= 0x0000ffff).

Definition at line 467 of file em_letimer.c .

References _LETIMER_REP0_REP0_MASK , _LETIMER_REP0_REP0_SHIFT , LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .

Referenced by MIC_init() .

void LETIMER_Reset ( LETIMER_TypeDef * letimer )

Reset LETIMER to the same state that it was in after a hardware reset.

Note
The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
Parameters
[in] letimer A pointer to the LETIMER peripheral register block.

Definition at line 521 of file em_letimer.c .

References _LETIMER_COMP0_RESETVALUE , _LETIMER_COMP1_RESETVALUE , _LETIMER_CTRL_RESETVALUE , _LETIMER_IEN_RESETVALUE , _LETIMER_IF_MASK , _LETIMER_REP0_RESETVALUE , _LETIMER_REP1_RESETVALUE , _LETIMER_SYNCBUSY_MASK , LETIMER_TypeDef::CMD , LETIMER_TypeDef::COMP0 , LETIMER_TypeDef::COMP1 , LETIMER_TypeDef::CTRL , LETIMER_TypeDef::IEN , LETIMER0 , LETIMER_CMD_CLEAR , LETIMER_CMD_CTO0 , LETIMER_CMD_CTO1 , LETIMER_CMD_STOP , LETIMER_IntClear() , LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .

__STATIC_INLINE uint32_t LETIMER_TopGet ( LETIMER_TypeDef * letimer )

Get the current LETIMER top value.

Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
Returns
The top value. This will be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.

Definition at line 321 of file em_letimer.h .

References LETIMER_TypeDef::COMP0 .

void LETIMER_TopSet ( LETIMER_TypeDef * letimer,
uint32_t value
)

Set the LETIMER top value.

Note
The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value.

If the LETIMER is not already configured to use a top value then this function will enable that functionality for the user.

Parameters
[in] letimer A pointer to the LETIMER peripheral register block.
[in] value The top value. This can be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.

Definition at line 591 of file em_letimer.c .

References LETIMER_TypeDef::CTRL , LETIMER_CompareSet() , LETIMER_CTRL_COMP0TOP , and LETIMER_SyncWait() .