LESENSE_CH_TypeDef Struct ReferenceDevicesDevices > | LESENSE
LESENSE_CH LESENSE CH Register
.
Definition at line
46
of file
efm32jg12b_lesense_ch.h
.
#include <
efm32jg12b_lesense_ch.h
>
Data Fields |
|
| __IOM uint32_t | EVAL |
| __IOM uint32_t | INTERACT |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | TIMING |
Field Documentation
| __IOM uint32_t LESENSE_CH_TypeDef::EVAL |
Scan Configuration
Definition at line
49
of file
efm32jg12b_lesense_ch.h
.
Referenced by LESENSE_ChannelSlidingWindow() , and LESENSE_ChannelStepDetection() .
| __IOM uint32_t LESENSE_CH_TypeDef::INTERACT |
Scan Configuration
Definition at line
48
of file
efm32jg12b_lesense_ch.h
.
| uint32_t LESENSE_CH_TypeDef::RESERVED0[1U] |
Reserved future
Definition at line
50
of file
efm32jg12b_lesense_ch.h
.
| __IOM uint32_t LESENSE_CH_TypeDef::TIMING |
Scan Configuration
Definition at line
47
of file
efm32jg12b_lesense_ch.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/
efm32jg12b_lesense_ch.h