ADC_TypeDef Struct ReferenceDevices > ADC
ADC Register Declaration
Definition at line
48
of file
efm32jg12b_adc.h
.
#include <
efm32jg12b_adc.h
>
Data Fields |
|
| __IM uint32_t | APORTCONFLICT |
| __IOM uint32_t | APORTMASTERDIS |
| __IM uint32_t | APORTREQ |
| __IOM uint32_t | BIASPROG |
| __IOM uint32_t | CAL |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CMPTHR |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [4U] |
| uint32_t | RESERVED2 [3U] |
| __IOM uint32_t | SCANCTRL |
| __IOM uint32_t | SCANCTRLX |
| __IM uint32_t | SCANDATA |
| __IM uint32_t | SCANDATAP |
| __IM uint32_t | SCANDATAX |
| __IM uint32_t | SCANDATAXP |
| __IOM uint32_t | SCANFIFOCLEAR |
| __IM uint32_t | SCANFIFOCOUNT |
| __IOM uint32_t | SCANINPUTSEL |
| __IOM uint32_t | SCANMASK |
| __IOM uint32_t | SCANNEGSEL |
| __IOM uint32_t | SINGLECTRL |
| __IOM uint32_t | SINGLECTRLX |
| __IM uint32_t | SINGLEDATA |
| __IM uint32_t | SINGLEDATAP |
| __IOM uint32_t | SINGLEFIFOCLEAR |
| __IM uint32_t | SINGLEFIFOCOUNT |
| __IM uint32_t | STATUS |
Field Documentation
| __IM uint32_t ADC_TypeDef::APORTCONFLICT |
APORT Conflict Status Register
Definition at line
77
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::APORTMASTERDIS |
APORT Bus Master Disable Register
Definition at line
82
of file
efm32jg12b_adc.h
.
| __IM uint32_t ADC_TypeDef::APORTREQ |
APORT Request Status Register
Definition at line
76
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::BIASPROG |
Bias Programming Register for Various Analog Blocks Used in ADC Operation
Definition at line
61
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitSingle() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::CAL |
Calibration Register
Definition at line
62
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::CMD |
Command Register
Definition at line
51
of file
efm32jg12b_adc.h
.
Referenced by ADC_Init() , ADC_InitScan() , ADC_InitSingle() , ADC_Reset() , and ADC_Start() .
| __IOM uint32_t ADC_TypeDef::CMPTHR |
Compare Threshold Register
Definition at line
60
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::CTRL |
Control Register
Definition at line
49
of file
efm32jg12b_adc.h
.
Referenced by ADC_Init() , ADC_InitScan() , ADC_InitSingle() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::IEN |
Interrupt Enable Register
Definition at line
66
of file
efm32jg12b_adc.h
.
Referenced by ADC_IntDisable() , ADC_IntEnable() , ADC_IntGetEnabled() , and ADC_Reset() .
| __IM uint32_t ADC_TypeDef::IF |
Interrupt Flag Register
Definition at line
63
of file
efm32jg12b_adc.h
.
Referenced by ADC_IntGet() , and ADC_IntGetEnabled() .
| __IOM uint32_t ADC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
65
of file
efm32jg12b_adc.h
.
Referenced by ADC_IntClear() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
64
of file
efm32jg12b_adc.h
.
Referenced by ADC_IntSet() .
| uint32_t ADC_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
50
of file
efm32jg12b_adc.h
.
| uint32_t ADC_TypeDef::RESERVED1[4U] |
Reserved for future use
Definition at line
71
of file
efm32jg12b_adc.h
.
| uint32_t ADC_TypeDef::RESERVED2[3U] |
Reserved for future use
Definition at line
75
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::SCANCTRL |
Scan Control Register
Definition at line
55
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SCANCTRLX |
Scan Control Register Continued
Definition at line
56
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SCANDATA |
Scan Conversion Result Data
Definition at line
68
of file
efm32jg12b_adc.h
.
Referenced by ADC_DataScanGet() .
| __IM uint32_t ADC_TypeDef::SCANDATAP |
Scan Sequence Result Data Peek Register
Definition at line
70
of file
efm32jg12b_adc.h
.
Referenced by ADC_DataScanPeek() .
| __IM uint32_t ADC_TypeDef::SCANDATAX |
Scan Sequence Result Data + Data Source Register
Definition at line
72
of file
efm32jg12b_adc.h
.
Referenced by ADC_DataIdScanGet() .
| __IM uint32_t ADC_TypeDef::SCANDATAXP |
Scan Sequence Result Data + Data Source Peek Register
Definition at line
73
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::SCANFIFOCLEAR |
Scan FIFO Clear Register
Definition at line
81
of file
efm32jg12b_adc.h
.
Referenced by ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SCANFIFOCOUNT |
Scan FIFO Count Register
Definition at line
79
of file
efm32jg12b_adc.h
.
| __IOM uint32_t ADC_TypeDef::SCANINPUTSEL |
Input Selection Register for Scan Mode
Definition at line
58
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SCANMASK |
Scan Sequence Input Mask Register
Definition at line
57
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SCANNEGSEL |
Negative Input Select Register for Scan
Definition at line
59
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SINGLECTRL |
Single Channel Control Register
Definition at line
53
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitSingle() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SINGLECTRLX |
Single Channel Control Register Continued
Definition at line
54
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitSingle() , and ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SINGLEDATA |
Single Conversion Result Data
Definition at line
67
of file
efm32jg12b_adc.h
.
Referenced by ADC_DataSingleGet() .
| __IM uint32_t ADC_TypeDef::SINGLEDATAP |
Single Conversion Result Data Peek Register
Definition at line
69
of file
efm32jg12b_adc.h
.
Referenced by ADC_DataSinglePeek() .
| __IOM uint32_t ADC_TypeDef::SINGLEFIFOCLEAR |
Single FIFO Clear Register
Definition at line
80
of file
efm32jg12b_adc.h
.
Referenced by ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SINGLEFIFOCOUNT |
Single FIFO Count Register
Definition at line
78
of file
efm32jg12b_adc.h
.
| __IM uint32_t ADC_TypeDef::STATUS |
Status Register
Definition at line
52
of file
efm32jg12b_adc.h
.
Referenced by ADC_InitScan() , and ADC_InitSingle() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/
efm32jg12b_adc.h