ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP

ACMP initialization structure.

Definition at line 733 of file em_acmp.h.

#include <em_acmp.h>

Data Fields

uint32_t biasProg
 
bool enable
 
bool fullBias
 
bool halfBias
 
ACMP_HysteresisLevel_TypeDef hysteresisLevel
 
bool inactiveValue
 
bool interruptOnFallingEdge
 
bool interruptOnRisingEdge
 
bool lowPowerReferenceEnabled
 
uint32_t vddLevel
 
ACMP_WarmTime_TypeDef warmTime
 

Field Documentation

uint32_t ACMP_Init_TypeDef::biasProg

Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.

Definition at line 748 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::enable

If true, ACMP is enabled after configuration.

Definition at line 823 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::fullBias

Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 737 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::halfBias

Half-bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 743 of file em_acmp.h.

Referenced by ACMP_Init().

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel

Hysteresis level.

Definition at line 788 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::inactiveValue

Inactive value emitted by ACMP during warmup.

Definition at line 804 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::interruptOnFallingEdge

Enable setting the interrupt flag on the falling edge.

Definition at line 752 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::interruptOnRisingEdge

Enable setting the interrupt flag on the rising edge.

Definition at line 756 of file em_acmp.h.

Referenced by ACMP_Init().

bool ACMP_Init_TypeDef::lowPowerReferenceEnabled

Low power reference enabled. This setting, if enabled, reduces the power used by the VDD and bandgap references.

Definition at line 809 of file em_acmp.h.

Referenced by ACMP_Init().

uint32_t ACMP_Init_TypeDef::vddLevel

VDD reference value. VDD_SCALED = VDD * VDDLEVEL * 50 mV/3.8 V. Valid values are in the 0-63 range.

Definition at line 819 of file em_acmp.h.

Referenced by ACMP_Init().

ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime

Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.

Definition at line 782 of file em_acmp.h.

Referenced by ACMP_Init().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/em_acmp.h