USB_EndpointDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB Endpoint Descriptor.
Definition at line 492
of file em_usb.h
.
#include <
em_usb.h
>
Data Fields | |
uint8_t | bDescriptorType |
uint8_t | bEndpointAddress |
uint8_t | bInterval |
uint8_t | bLength |
uint8_t | bmAttributes |
uint16_t | wMaxPacketSize |
Field Documentation
uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType |
Constant ENDPOINT Descriptor Type
Definition at line 494
of file em_usb.h
.
Referenced by USBH_PrintEndpointDescriptor().
uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress |
The address of the endpoint
Definition at line 495
of file em_usb.h
.
Referenced by USBD_Init(), USBH_AssignHostChannel(), and USBH_PrintEndpointDescriptor().
uint8_t USB_EndpointDescriptor_TypeDef::bInterval |
Interval for polling EP for data transfers
Definition at line 498
of file em_usb.h
.
Referenced by USBD_Init(), USBH_PrintEndpointDescriptor(), USBH_Read(), and USBH_Write().
uint8_t USB_EndpointDescriptor_TypeDef::bLength |
Size of this descriptor in bytes
Definition at line 493
of file em_usb.h
.
Referenced by USBH_PrintEndpointDescriptor().
uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes |
This field describes the endpoint attributes
Definition at line 496
of file em_usb.h
.
Referenced by USBD_Init(), USBH_AssignHostChannel(), and USBH_PrintEndpointDescriptor().
uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize |
Maximum packet size for the endpoint
Definition at line 497
of file em_usb.h
.
Referenced by USBD_Init(), USBH_AssignHostChannel(), and USBH_PrintEndpointDescriptor().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/middleware/usb_gecko/inc/
em_usb.h