DAC_Init_TypeDef Struct ReferenceEMLIB > DAC
DAC initialization structure, common for both channels.
Definition at line
134
of file
em_dac.h
.
#include <
em_dac.h
>
Data Fields |
|
bool | ch0ResetPre |
DAC_ConvMode_TypeDef | convMode |
bool | diff |
bool | lpEnable |
bool | outEnablePRS |
DAC_Output_TypeDef | outMode |
uint8_t | prescale |
DAC_Ref_TypeDef | reference |
DAC_Refresh_TypeDef | refresh |
bool | sineEnable |
Field Documentation
bool DAC_Init_TypeDef::ch0ResetPre |
Enable/disable reset of prescaler on ch0 start.
Definition at line
157
of file
em_dac.h
.
Referenced by DAC_Init() .
DAC_ConvMode_TypeDef DAC_Init_TypeDef::convMode |
bool DAC_Init_TypeDef::diff |
Select if single ended or differential mode.
Definition at line
166
of file
em_dac.h
.
Referenced by DAC_Init() .
bool DAC_Init_TypeDef::lpEnable |
Enable/disable use of low pass filter on output.
Definition at line
154
of file
em_dac.h
.
bool DAC_Init_TypeDef::outEnablePRS |
Enable/disable output enable control by CH1 PRS signal.
Definition at line
160
of file
em_dac.h
.
Referenced by DAC_Init() .
DAC_Output_TypeDef DAC_Init_TypeDef::outMode |
uint8_t DAC_Init_TypeDef::prescale |
Prescaler used to get DAC clock. Derived as follows: DACclk=HFPERclk/(2^prescale). The DAC clock should be <= 1MHz.
Definition at line
151
of file
em_dac.h
.
Referenced by DAC_Init() .
DAC_Ref_TypeDef DAC_Init_TypeDef::reference |
DAC_Refresh_TypeDef DAC_Init_TypeDef::refresh |
Refresh interval. Only used if REFREN bit set for a DAC channel.
Definition at line
136
of file
em_dac.h
.
Referenced by DAC_Init() .
bool DAC_Init_TypeDef::sineEnable |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_dac.h