RTC_TypeDef Struct ReferenceDevices > EFM32LG_RTC
Definition at line
47
of file
efm32lg_rtc.h
.
Data Fields |
|
| __IOM uint32_t | CNT |
| __IOM uint32_t | COMP0 |
| __IOM uint32_t | COMP1 |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | FREEZE |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IM uint32_t | SYNCBUSY |
Field Documentation
| __IOM uint32_t RTC_TypeDef::CNT |
Counter Value Register
Definition at line
49
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::COMP0 |
Compare Value Register 0
Definition at line
50
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::COMP1 |
Compare Value Register 1
Definition at line
51
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::CTRL |
Control Register
Definition at line
48
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::FREEZE |
Freeze Register
Definition at line
57
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::IEN |
Interrupt Enable Register
Definition at line
55
of file
efm32lg_rtc.h
.
| __IM uint32_t RTC_TypeDef::IF |
Interrupt Flag Register
Definition at line
52
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
54
of file
efm32lg_rtc.h
.
| __IOM uint32_t RTC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
53
of file
efm32lg_rtc.h
.
| __IM uint32_t RTC_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line
58
of file
efm32lg_rtc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32LG/Include/
efm32lg_rtc.h