PCNT_Filter_TypeDef Struct ReferenceEMLIB > PCNT
Filter initialization structure
Definition at line
264
of file
em_pcnt.h
.
#include <
em_pcnt.h
>
Data Fields |
|
| uint8_t | filtLen |
| bool | flutterrm |
Field Documentation
| uint8_t PCNT_Filter_TypeDef::filtLen |
Used only in OVSINGLE and OVSQUAD1X-4X modes. To use this, enable filter by setting filter to true during PCNT_Init() . Filter length = (filtLen + 5) LFACLK cycles.
Definition at line
267
of file
em_pcnt.h
.
Referenced by PCNT_FilterConfiguration() .
| bool PCNT_Filter_TypeDef::flutterrm |
When set, removes flutter from Quaddecoder inputs S0IN and S1IN. Available only in OVSQUAD1X-4X modes.
Definition at line
271
of file
em_pcnt.h
.
Referenced by PCNT_FilterConfiguration() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_pcnt.h