USART_PrsTriggerInit_TypeDef Struct ReferenceEMLIB > USART
USART PRS trigger enable.
Definition at line 335
of file em_usart.h
.
#include <
em_usart.h
>
Data Fields | |
bool | autoTxTriggerEnable |
USART_PRS_Channel_t | prsTriggerChannel |
bool | rxTriggerEnable |
bool | txTriggerEnable |
Field Documentation
bool USART_PrsTriggerInit_TypeDef::autoTxTriggerEnable |
USART_PRS_Channel_t USART_PrsTriggerInit_TypeDef::prsTriggerChannel |
PRS channel to be used to trigger auto transmission.
Definition at line 345
of file em_usart.h
.
Referenced by USART_InitPrsTrigger().
bool USART_PrsTriggerInit_TypeDef::rxTriggerEnable |
Trigger receive via PRS channel.
Definition at line 341
of file em_usart.h
.
Referenced by USART_InitPrsTrigger().
bool USART_PrsTriggerInit_TypeDef::txTriggerEnable |
Trigger transmit via PRS channel.
Definition at line 343
of file em_usart.h
.
Referenced by USART_InitPrsTrigger().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_usart.h