GPIOINTEMDRV
Detailed Description
GPIOINT General Purpose Input/Output Interrupt dispatcher.
The source files for the GPIO interrupt dispatcher library resides in the emdrv/gpiointerrupt folder, and are named
gpiointerrupt.c
and
gpiointerrupt.h
.
Introduction
EFM32/EZR32/EFR32 has two GPIO interrupts lines, Odd and Even. If more than two interrupts are used then interrupt routine must dispatch from a callback register. This module provides small dispatcher for both GPIO interrupts enabling handling of up to 16 GPIO pin interrupts.
It is up to the user to configure and enable interrupt on given pin. This can be done using the GPIO library (emlib). This module handles the dispatch register and clearing of interrupt flags.
In order to use this dispatcher, it has to be initialized first by calling GPIOINT_Init() . Then each pin interrupt number must be configured by first registering the callback function for given interrupt number and then configure and enabling the interrupt number in the GPIO module.
The API
This section contain brief descriptions of the functions in the API. You will find detailed information on parameters by clicking on the hyperlinked function names.
Your application code must include one header file:
gpiointerrupt.h
.
GPIOINT_Init()
This functions initializes the dispatcher register. Typically GPIOINT_Init() is called once in your startup code.
GPIOINT_CallbackRegister()
Register a callback function on a pin interrupt number.
GPIOINT_CallbackUnRegister()
Un-register a callback function on a pin interrupt number.
Example
em_gpio.h
"
em_int.h
"
gpiointerrupt.h
"
Typedefs |
|
typedef void(* | GPIOINT_IrqCallbackPtr_t ) (uint8_t intNo) |
GPIO interrupt callback function pointer.
|
|
Functions |
|
void | GPIOINT_CallbackRegister (uint8_t intNo, GPIOINT_IrqCallbackPtr_t callbackPtr) |
Registers user callback for given pin interrupt number.
|
|
static __INLINE void | GPIOINT_CallbackUnRegister (uint8_t intNo) |
Unregisters user callback for given pin interrupt number.
|
|
void | GPIOINT_Init (void) |
Initialization of GPIOINT module.
|
|
Typedef Documentation
typedef void(* GPIOINT_IrqCallbackPtr_t) (uint8_t intNo) |
GPIO interrupt callback function pointer.
Parameters:
- intNo - The pin interrupt number the callback function is invoked for.
Definition at line
61
of file
gpiointerrupt.h
.
Function Documentation
void GPIOINT_CallbackRegister | ( | uint8_t |
intNo,
|
GPIOINT_IrqCallbackPtr_t |
callbackPtr
|
||
) |
Registers user callback for given pin interrupt number.
Use this function to register a callback which shall be called upon interrupt generated for a given pin interrupt number. Interrupt itself must be configured externally. Function overwrites previously registered callback.
- Parameters
-
[in] pin
Pin number for the callback. [in] callbackPtr
A pointer to callback function.
Definition at line
101
of file
gpiointerrupt.c
.
References CORE_ATOMIC_SECTION , GPIO_EVEN_IRQHandler() , GPIO_IntClear() , GPIO_IntGetEnabled() , GPIO_ODD_IRQHandler() , and SL_CTZ() .
Referenced by BOARD_alsSetIRQCallback() , BOARD_gasSensorSetIRQCallback() , BOARD_hallSensorSetIRQCallback() , BOARD_imuSetIRQCallback() , BOARD_pushButton0SetIRQCallback() , BOARD_pushButton1SetIRQCallback() , ezradio_hal_GpioInit() , GPIOINT_CallbackUnRegister() , and UARTDRV_DeInit() .
|
static |
Unregisters user callback for given pin interrupt number.
Use this function to unregister a callback.
- Parameters
-
[in] intNo
Pin interrupt number for the callback.
Definition at line
81
of file
gpiointerrupt.h
.
References GPIOINT_CallbackRegister() .