LDMA_Init_t Struct ReferenceEMLIB > LDMA
LDMA initialization configuration structure.
Definition at line 877
of file em_ldma.h
.
#include <
em_ldma.h
>
Data Fields | |
uint8_t | ldmaInitCtrlNumFixed |
uint8_t | ldmaInitCtrlSyncPrsClrEn |
uint8_t | ldmaInitCtrlSyncPrsSetEn |
uint8_t | ldmaInitIrqPriority |
Field Documentation
uint8_t LDMA_Init_t::ldmaInitCtrlNumFixed |
Arbitration mode separator.
Definition at line 878
of file em_ldma.h
.
Referenced by DMADRV_Init(), and LDMA_Init().
uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsClrEn |
uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsSetEn |
uint8_t LDMA_Init_t::ldmaInitIrqPriority |
LDMA IRQ priority (0..7).
Definition at line 881
of file em_ldma.h
.
Referenced by DMADRV_Init(), and LDMA_Init().
The documentation for this struct was generated from the following file:
- C:/repos/super/platform/emlib/inc/
em_ldma.h