BATTERY_TypeDef Struct ReferenceKit Drivers > SegmentLcd

Defines segment COM and BIT fields for Battery (suited for Anim)

Definition at line 128 of file segmentlcd.c .

Data Fields

uint8_t bit [4]
uint8_t com [4]

Field Documentation

uint8_t BATTERY_TypeDef::bit[4]

LCD bit number

Definition at line 130 of file segmentlcd.c .

uint8_t BATTERY_TypeDef::com[4]

LCD COM line (for multiplexing)

Definition at line 129 of file segmentlcd.c .


The documentation for this struct was generated from the following file:
  • C:/repos/super/hardware/kit/common/drivers/ segmentlcd.c