ARRAY_TypeDef Struct ReferenceKit Drivers > SegmentLcd

Defines segment COM and BIT fields for array.

Definition at line 136 of file segmentlcd.c .

Data Fields

uint8_t bit [35]
uint8_t com [35]

Field Documentation

uint8_t ARRAY_TypeDef::bit[35]

LCD bit number

Definition at line 138 of file segmentlcd.c .

uint8_t ARRAY_TypeDef::com[35]

LCD COM line (for multiplexing)

Definition at line 137 of file segmentlcd.c .


The documentation for this struct was generated from the following file:
  • C:/repos/super/hardware/kit/common/drivers/ segmentlcd.c