MSC_EccConfig_TypeDef Struct ReferenceEMLIB > MSC

ECC configuration.

Definition at line 237 of file em_msc.h .

#include < em_msc.h >

Data Fields

uint32_t dmaChannels [2]
bool enableEccBank [ MSC_ECC_BANKS ]

Field Documentation

uint32_t MSC_EccConfig_TypeDef::dmaChannels[2]

Array of 2 DMA channel numbers to use for ECC initialization.

Definition at line 242 of file em_msc.h .

Referenced by MSC_EccConfigSet() .

bool MSC_EccConfig_TypeDef::enableEccBank[ MSC_ECC_BANKS ]

Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.

Definition at line 238 of file em_msc.h .

Referenced by MSC_EccConfigSet() .


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/ em_msc.h