EZRADIODRV_PacketTxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin
EzRadio transmit plug-in instance initialization and handler structure.
Definition at line 98
of file ezradio_transmit_plugin.h
.
#include <
ezradio_transmit_plugin.h
>
Data Fields | |
uint8_t | channel |
Transmission channel. | |
EZRADIODRV_PacketLengthConfig_t | lenConfig |
Packet length configuration. | |
uint16_t | pktId |
Packet ID. | |
EZRADIODRV_TransmitPacketType_t | pktType |
Packet type. | |
EZRADIODRV_Callback_t | userCallback |
User callback. | |
The documentation for this struct was generated from the following file:
- C:/repos/super/platform/emdrv/ezradiodrv/plugins/inc/
ezradio_transmit_plugin.h