BURTC
Detailed Description
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
Data Structures |
|
struct | BURTC_Init_TypeDef |
Macros |
|
#define | BURTC_INIT_DEFAULT |
#define | burtcClkDiv_1 1 |
#define | burtcClkDiv_128 128 |
#define | burtcClkDiv_16 16 |
#define | burtcClkDiv_2 2 |
#define | burtcClkDiv_32 32 |
#define | burtcClkDiv_4 4 |
#define | burtcClkDiv_64 64 |
#define | burtcClkDiv_8 8 |
Functions |
|
uint32_t | BURTC_ClockFreqGet (void) |
uint32_t | BURTC_CompareGet (unsigned int comp) |
Get the BURTC compare value.
|
|
void | BURTC_CompareSet (unsigned int comp, uint32_t value) |
Set BURTC compare channel.
|
|
__STATIC_INLINE uint32_t | BURTC_CounterGet (void) |
Get BURTC counter.
|
|
void | BURTC_CounterReset (void) |
Reset counter.
|
|
void | BURTC_Enable (bool enable) |
Enable or Disable BURTC peripheral.
|
|
void | BURTC_Init (const BURTC_Init_TypeDef *burtcInit) |
Initialize BURTC.
|
|
__STATIC_INLINE void | BURTC_IntClear (uint32_t flags) |
Clear one or more pending BURTC interrupts.
|
|
__STATIC_INLINE void | BURTC_IntDisable (uint32_t flags) |
Disable one or more BURTC interrupts.
|
|
__STATIC_INLINE void | BURTC_IntEnable (uint32_t flags) |
Enable one or more BURTC interrupts.
|
|
__STATIC_INLINE uint32_t | BURTC_IntGet (void) |
Get pending BURTC interrupt flags.
|
|
__STATIC_INLINE uint32_t | BURTC_IntGetEnabled (void) |
Get enabled and pending BURTC interrupt flags.
|
|
__STATIC_INLINE void | BURTC_IntSet (uint32_t flags) |
Set one or more pending BURTC interrupts from SW.
|
|
__STATIC_INLINE void | BURTC_Lock (void) |
Lock BURTC registers, will protect from writing new config settings.
|
|
void | BURTC_Reset (void) |
Restore BURTC to reset state.
|
|
__STATIC_INLINE void | BURTC_Start (void) |
Start BURTC counter.
|
|
__STATIC_INLINE uint32_t | BURTC_Status (void) |
Status of BURTC RAM, timestamp and LP Mode.
|
|
__STATIC_INLINE void | BURTC_Stop (void) |
Stop the BURTC counter.
|
|
__STATIC_INLINE void | BURTC_SyncWait (void) |
Wait for the BURTC to complete all synchronization of register changes and commands.
|
|
__STATIC_INLINE void | BURTC_Unlock (void) |
Unlock BURTC registers, enable write access to change configuration.
|
|
Macro Definition Documentation
#define BURTC_INIT_DEFAULT |
Default configuration for BURTC init structure
Definition at line
155
of file
em_burtc.h
.
#define burtcClkDiv_1 1 |
BURTC clock divisors. These values are valid for the BURTC prescaler. Divide clock by 1.
Definition at line
60
of file
em_burtc.h
.
#define burtcClkDiv_128 128 |
Divide clock by 128.
Definition at line
67
of file
em_burtc.h
.
#define burtcClkDiv_16 16 |
Divide clock by 16.
Definition at line
64
of file
em_burtc.h
.
#define burtcClkDiv_2 2 |
Divide clock by 2.
Definition at line
61
of file
em_burtc.h
.
#define burtcClkDiv_32 32 |
Divide clock by 32.
Definition at line
65
of file
em_burtc.h
.
#define burtcClkDiv_4 4 |
Divide clock by 4.
Definition at line
62
of file
em_burtc.h
.
#define burtcClkDiv_64 64 |
Divide clock by 64.
Definition at line
66
of file
em_burtc.h
.
#define burtcClkDiv_8 8 |
Divide clock by 8.
Definition at line
63
of file
em_burtc.h
.
Function Documentation
uint32_t BURTC_CompareGet | ( | unsigned int |
comp
|
) |
Get the BURTC compare value.
- Parameters
-
[in] comp
Compare the channel index value, must be 0 for Giant/Leopard Gecko.
- Returns
- The currently configured value for this compare channel.
Definition at line
300
of file
em_burtc.c
.
void BURTC_CompareSet | ( | unsigned int |
comp,
|
uint32_t |
value
|
||
) |
Set BURTC compare channel.
- Parameters
-
[in] comp
Compare the channel index, must be 0 for current devices. [in] value
New compare value.
Definition at line
270
of file
em_burtc.c
.
__STATIC_INLINE uint32_t BURTC_CounterGet | ( | void |
|
) |
Get BURTC counter.
- Returns
- BURTC counter value
Definition at line
372
of file
em_burtc.h
.
void BURTC_Enable | ( | bool |
enable
|
) |
Enable or Disable BURTC peripheral.
- Parameters
-
[in] enable
true to enable, false to disable.
Definition at line
223
of file
em_burtc.c
.
References BURTC_Stop() , and BURTC_SyncWait() .
Referenced by BURTC_Init() .
void BURTC_Init | ( | const BURTC_Init_TypeDef * |
burtcInit
|
) |
Initialize BURTC.
Configures the BURTC peripheral.
- Note
-
Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
* RMU_ResetControl(rmuResetBU, rmuResetModeClear); *
Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
- Parameters
-
[in] burtcInit
A pointer to the BURTC initialization structure.
Definition at line
128
of file
em_burtc.c
.
References BURTC_Enable() , BURTC_IntClear() , BURTC_Start() , BURTC_SyncWait() , BURTC_Init_TypeDef::clkDiv , BURTC_Init_TypeDef::compare0Top , BURTC_Init_TypeDef::debugRun , BURTC_Init_TypeDef::em4comp , BURTC_Init_TypeDef::em4overflow , and BURTC_Init_TypeDef::start .
__STATIC_INLINE void BURTC_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending BURTC interrupts.
- Parameters
-
[in] flags
BURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
179
of file
em_burtc.h
.
Referenced by BURTC_Init() .
__STATIC_INLINE void BURTC_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more BURTC interrupts.
- Parameters
-
[in] flags
BURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
197
of file
em_burtc.h
.
__STATIC_INLINE void BURTC_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more BURTC interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
-
[in] flags
BURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
220
of file
em_burtc.h
.
__STATIC_INLINE uint32_t BURTC_IntGet | ( | void |
|
) |
Get pending BURTC interrupt flags.
- Note
- This function does not clear the event bits.
- Returns
- Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
Definition at line
240
of file
em_burtc.h
.
__STATIC_INLINE uint32_t BURTC_IntGetEnabled | ( | void |
|
) |
Get enabled and pending BURTC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
Definition at line
257
of file
em_burtc.h
.
__STATIC_INLINE void BURTC_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending BURTC interrupts from SW.
- Parameters
-
[in] flags
BURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
Definition at line
277
of file
em_burtc.h
.
void BURTC_Reset | ( | void |
|
) |
Restore BURTC to reset state.
- Note
- Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
Definition at line
336
of file
em_burtc.c
.
References BURTC_Stop() , BURTC_SyncWait() , BUS_RegBitRead() , and BUS_RegBitWrite() .
__STATIC_INLINE void BURTC_Start | ( | void |
|
) |
Start BURTC counter.
This function will send a start command to the BURTC peripheral. The BURTC peripheral will use some LF clock ticks before the command is executed. The BURTC_SyncWait() function can be used to wait for the start command to be executed.
- Note
- This function requires the BURTC to be enabled.
Definition at line
340
of file
em_burtc.h
.
References BURTC_SyncWait() .
Referenced by BURTC_CounterReset() , and BURTC_Init() .
__STATIC_INLINE uint32_t BURTC_Status | ( | void |
|
) |
Status of BURTC RAM, timestamp and LP Mode.
- Returns
- A mask logially OR-ed status bits
Definition at line
292
of file
em_burtc.h
.
__STATIC_INLINE void BURTC_Stop | ( | void |
|
) |
Stop the BURTC counter.
This function will send a stop command to the BURTC peripheral. The BURTC peripheral will use some LF clock ticks before the command is executed. The BURTC_SyncWait() function can be used to wait for the stop command to be executed.
- Note
- This function requires the BURTC to be enabled.
Definition at line
359
of file
em_burtc.h
.
References BURTC_SyncWait() .
Referenced by BURTC_CounterReset() , BURTC_Enable() , and BURTC_Reset() .