IADC_InitScan_t Struct Reference

IADC scan init structure

Definition at line 699 of file em_iadc.h .

#include < em_iadc.h >

Data Fields

IADC_Alignment_t alignment
uint8_t dataValidLevel
bool fifoDmaWakeup
bool showId
bool start
IADC_TriggerAction_t triggerAction
IADC_TriggerSel_t triggerSelect

Field Documentation

IADC_Alignment_t IADC_InitScan_t::alignment

Alignment of data in FIFO.

Definition at line 700 of file em_iadc.h .

Referenced by IADC_initScan() .

uint8_t IADC_InitScan_t::dataValidLevel

Data valid level before requesting DMA transfer.

Definition at line 702 of file em_iadc.h .

Referenced by IADC_initScan() .

bool IADC_InitScan_t::fifoDmaWakeup

Wake-up DMA when FIFO reaches data valid level.

Definition at line 703 of file em_iadc.h .

Referenced by IADC_initScan() .

bool IADC_InitScan_t::showId

Tag FIFO entry with scan table entry id.

Definition at line 701 of file em_iadc.h .

Referenced by IADC_initScan() .

bool IADC_InitScan_t::start

Start scan immediately.

Definition at line 706 of file em_iadc.h .

Referenced by IADC_initScan() .

IADC_TriggerAction_t IADC_InitScan_t::triggerAction

Trigger action.

Definition at line 705 of file em_iadc.h .

Referenced by IADC_initScan() .

IADC_TriggerSel_t IADC_InitScan_t::triggerSelect

Trigger selection.

Definition at line 704 of file em_iadc.h .

Referenced by IADC_initScan() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_iadc.h