LFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.
Definition at line
495
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
bool | agcEn |
uint8_t | capTune |
bool | disOnDemand |
bool | failDetEM4WUEn |
bool | failDetEn |
bool | forceEn |
uint8_t | gain |
bool | highAmplitudeEn |
CMU_LfxoOscMode_TypeDef | mode |
bool | regLock |
CMU_LfxoStartupDelay_TypeDef | timeout |
Field Documentation
bool CMU_LFXOInit_TypeDef::agcEn |
uint8_t CMU_LFXOInit_TypeDef::capTune |
Internal capacitance tuning.
Definition at line
497
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_LFXOInit() .
bool CMU_LFXOInit_TypeDef::disOnDemand |
Disable on-demand requests.
Definition at line
504
of file
em_cmu.h
.
Referenced by CMU_LFXOInit() .
bool CMU_LFXOInit_TypeDef::failDetEM4WUEn |
EM4 wakeup on failure enable.
Definition at line
502
of file
em_cmu.h
.
Referenced by CMU_LFXOInit() .
bool CMU_LFXOInit_TypeDef::failDetEn |
Oscillator failure detection enable.
Definition at line
503
of file
em_cmu.h
.
Referenced by CMU_LFXOInit() .
bool CMU_LFXOInit_TypeDef::forceEn |
uint8_t CMU_LFXOInit_TypeDef::gain |
bool CMU_LFXOInit_TypeDef::highAmplitudeEn |
CMU_LfxoOscMode_TypeDef CMU_LFXOInit_TypeDef::mode |
bool CMU_LFXOInit_TypeDef::regLock |
CMU_LfxoStartupDelay_TypeDef CMU_LFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/emlib/inc/
em_cmu.h