SE_Status_t Struct Reference

Definition at line 378 of file em_se.h .

Data Fields

uint32_t bootStatus
SE_DebugStatus_t debugStatus
uint32_t hostFwVersion
bool secureBootEnabled
uint32_t seFwVersion

Field Documentation

uint32_t SE_Status_t::bootStatus

Boot status code / error code (Bits [7:0]).

Definition at line 380 of file em_se.h .

Referenced by SE_getStatus() .

SE_DebugStatus_t SE_Status_t::debugStatus

Debug lock status.

Definition at line 386 of file em_se.h .

Referenced by SE_getStatus() .

uint32_t SE_Status_t::hostFwVersion

Host firmware version (if available).

Definition at line 384 of file em_se.h .

Referenced by SE_getStatus() .

bool SE_Status_t::secureBootEnabled

Secure boot enabled.

Definition at line 388 of file em_se.h .

Referenced by SE_getStatus() .

uint32_t SE_Status_t::seFwVersion

SE firmware version.

Definition at line 382 of file em_se.h .

Referenced by SE_getStatus() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_se.h