ACMP_CapsenseInit_TypeDef Struct Reference

Capsense initialization structure.

Definition at line 605 of file em_acmp.h .

#include < em_acmp.h >

Data Fields

uint32_t biasProg
bool enable
ACMP_HysteresisLevel_TypeDef hysteresisLevel
ACMP_CapsenseResistor_TypeDef resistor
uint32_t vrefDiv

Field Documentation

uint32_t ACMP_CapsenseInit_TypeDef::biasProg

Bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 620 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() , and CAPLESENSE_setupACMP() .

bool ACMP_CapsenseInit_TypeDef::enable

If true, ACMP is enabled after configuration.

Definition at line 679 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel

Hysteresis level.

Definition at line 631 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor

A resistor used in the capacative sensing circuit. For values see the device data sheet.

Definition at line 642 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

uint32_t ACMP_CapsenseInit_TypeDef::vrefDiv

VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.

Definition at line 653 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_acmp.h