RTCC_Init_TypeDef Struct Reference

RTCC initialization structure.

Definition at line 213 of file em_rtcc.h .

#include < em_rtcc.h >

Data Fields

bool cntWrapOnCCV1
bool debugRun
bool enable
bool precntWrapOnCCV0
RTCC_CntPresc_TypeDef presc
RTCC_PrescMode_TypeDef prescMode

Field Documentation

bool RTCC_Init_TypeDef::cntWrapOnCCV1

Enable/disable counter wrap on ch. 1 CCV value.

Definition at line 224 of file em_rtcc.h .

Referenced by RTCC_Init() .

bool RTCC_Init_TypeDef::debugRun

Enable/disable timer counting during debug halt.

Definition at line 218 of file em_rtcc.h .

Referenced by RTCC_Init() .

bool RTCC_Init_TypeDef::enable

Enable/disable counting when initialization is completed.

Definition at line 215 of file em_rtcc.h .

Referenced by RTCC_Init() .

bool RTCC_Init_TypeDef::precntWrapOnCCV0

Enable/disable pre-counter wrap on ch. 0 CCV value.

Definition at line 221 of file em_rtcc.h .

Referenced by RTCC_Init() .

RTCC_CntPresc_TypeDef RTCC_Init_TypeDef::presc

Counter prescaler.

Definition at line 227 of file em_rtcc.h .

Referenced by RTCC_Init() , and RTCDRV_Init() .

RTCC_PrescMode_TypeDef RTCC_Init_TypeDef::prescMode

Prescaler mode.

Definition at line 230 of file em_rtcc.h .

Referenced by RTCC_Init() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_rtcc.h