GPIO
Detailed Description
General Purpose Input/Output (GPIO) API.
This module contains functions to control the GPIO peripheral of Silicon Labs 32-bit MCUs and SoCs. The GPIO peripheral is used for pin configuration and direct pin manipulation and sensing as well as routing for peripheral pin connections.
Enumerations |
|
enum |
GPIO_Mode_TypeDef
{
gpioModeDisabled = _GPIO_P_MODEL_MODE0_DISABLED, gpioModeInput = _GPIO_P_MODEL_MODE0_INPUT, gpioModeInputPull = _GPIO_P_MODEL_MODE0_INPUTPULL, gpioModeInputPullFilter = _GPIO_P_MODEL_MODE0_INPUTPULLFILTER, gpioModePushPull = _GPIO_P_MODEL_MODE0_PUSHPULL, gpioModePushPullAlternate = _GPIO_P_MODEL_MODE0_PUSHPULLALT, gpioModeWiredOr = _GPIO_P_MODEL_MODE0_WIREDOR, gpioModeWiredOrPullDown = _GPIO_P_MODEL_MODE0_WIREDORPULLDOWN, gpioModeWiredAnd = _GPIO_P_MODEL_MODE0_WIREDAND, gpioModeWiredAndFilter = _GPIO_P_MODEL_MODE0_WIREDANDFILTER, gpioModeWiredAndPullUp = _GPIO_P_MODEL_MODE0_WIREDANDPULLUP, gpioModeWiredAndPullUpFilter = _GPIO_P_MODEL_MODE0_WIREDANDPULLUPFILTER, gpioModeWiredAndAlternate = _GPIO_P_MODEL_MODE0_WIREDANDALT, gpioModeWiredAndAlternateFilter = _GPIO_P_MODEL_MODE0_WIREDANDALTFILTER, gpioModeWiredAndAlternatePullUp = _GPIO_P_MODEL_MODE0_WIREDANDALTPULLUP, gpioModeWiredAndAlternatePullUpFilter = _GPIO_P_MODEL_MODE0_WIREDANDALTPULLUPFILTER } |
enum | GPIO_Port_TypeDef |
Functions |
|
void | GPIO_DbgLocationSet (unsigned int location) |
Sets the pin location of the debug pins (Serial Wire interface).
|
|
__STATIC_INLINE void | GPIO_DbgSWDClkEnable (bool enable) |
Enable/disable serial wire clock pin.
|
|
__STATIC_INLINE void | GPIO_DbgSWDIOEnable (bool enable) |
Enable/disable serial wire data I/O pin.
|
|
__STATIC_INLINE void | GPIO_DbgSWOEnable (bool enable) |
Enable/Disable serial wire output pin.
|
|
__STATIC_INLINE void | GPIO_EM4DisablePinWakeup (uint32_t pinmask) |
Disable GPIO pin wake-up from EM4.
|
|
void | GPIO_EM4EnablePinWakeup (uint32_t pinmask, uint32_t polaritymask) |
Enable GPIO pin wake-up from EM4. When the function exits, EM4 mode can be safely entered.
|
|
__STATIC_INLINE uint32_t | GPIO_EM4GetPinWakeupCause (void) |
Check which GPIO pin(s) that caused a wake-up from EM4.
|
|
__STATIC_INLINE void | GPIO_EM4SetPinRetention (bool enable) |
Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.
|
|
void | GPIO_ExtIntConfig ( GPIO_Port_TypeDef port, unsigned int pin, unsigned int intNo, bool risingEdge, bool fallingEdge, bool enable) |
Configure the GPIO external pin interrupt.
|
|
__STATIC_INLINE void | GPIO_InputSenseSet (uint32_t val, uint32_t mask) |
Enable/disable input sensing.
|
|
__STATIC_INLINE void | GPIO_IntClear (uint32_t flags) |
Clear one or more pending GPIO interrupts.
|
|
__STATIC_INLINE void | GPIO_IntConfig ( GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable) |
Configure GPIO interrupt.
|
|
__STATIC_INLINE void | GPIO_IntDisable (uint32_t flags) |
Disable one or more GPIO interrupts.
|
|
__STATIC_INLINE void | GPIO_IntEnable (uint32_t flags) |
Enable one or more GPIO interrupts.
|
|
__STATIC_INLINE uint32_t | GPIO_IntGet (void) |
Get pending GPIO interrupts.
|
|
__STATIC_INLINE uint32_t | GPIO_IntGetEnabled (void) |
Get enabled and pending GPIO interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
__STATIC_INLINE void | GPIO_IntSet (uint32_t flags) |
Set one or more pending GPIO interrupts from SW.
|
|
__STATIC_INLINE void | GPIO_Lock (void) |
Locks the GPIO configuration.
|
|
__STATIC_INLINE unsigned int | GPIO_PinInGet ( GPIO_Port_TypeDef port, unsigned int pin) |
Read the pad value for a single pin in a GPIO port.
|
|
GPIO_Mode_TypeDef | GPIO_PinModeGet ( GPIO_Port_TypeDef port, unsigned int pin) |
Get the mode for a GPIO pin.
|
|
void | GPIO_PinModeSet ( GPIO_Port_TypeDef port, unsigned int pin, GPIO_Mode_TypeDef mode, unsigned int out) |
Set the mode for a GPIO pin.
|
|
__STATIC_INLINE void | GPIO_PinOutClear ( GPIO_Port_TypeDef port, unsigned int pin) |
Set a single pin in GPIO data out port register to 0.
|
|
__STATIC_INLINE unsigned int | GPIO_PinOutGet ( GPIO_Port_TypeDef port, unsigned int pin) |
Get current setting for a pin in a GPIO port data out register.
|
|
__STATIC_INLINE void | GPIO_PinOutSet ( GPIO_Port_TypeDef port, unsigned int pin) |
Set a single pin in GPIO data out register to 1.
|
|
__STATIC_INLINE void | GPIO_PinOutToggle ( GPIO_Port_TypeDef port, unsigned int pin) |
Toggle a single pin in GPIO port data out register.
|
|
__STATIC_INLINE uint32_t | GPIO_PortInGet ( GPIO_Port_TypeDef port) |
Read the pad values for GPIO port.
|
|
__STATIC_INLINE void | GPIO_PortOutClear ( GPIO_Port_TypeDef port, uint32_t pins) |
Set bits in DOUT register for a port to 0.
|
|
__STATIC_INLINE uint32_t | GPIO_PortOutGet ( GPIO_Port_TypeDef port) |
Get current setting for a GPIO port data out register.
|
|
__STATIC_INLINE void | GPIO_PortOutSet ( GPIO_Port_TypeDef port, uint32_t pins) |
Set bits GPIO data out register to 1.
|
|
__STATIC_INLINE void | GPIO_PortOutSetVal ( GPIO_Port_TypeDef port, uint32_t val, uint32_t mask) |
Set GPIO port data out register.
|
|
__STATIC_INLINE void | GPIO_PortOutToggle ( GPIO_Port_TypeDef port, uint32_t pins) |
Toggle pins in GPIO port data out register.
|
|
__STATIC_INLINE void | GPIO_SlewrateSet ( GPIO_Port_TypeDef port, uint32_t slewrate, uint32_t slewrateAlt) |
Set slewrate for pins on a GPIO port.
|
|
__STATIC_INLINE void | GPIO_Unlock (void) |
Unlocks the GPIO configuration.
|
|
Enumeration Type Documentation
enum GPIO_Mode_TypeDef |
Pin mode. For more details on each mode, refer to the reference manual.
Definition at line
552
of file
em_gpio.h
.
enum GPIO_Port_TypeDef |
GPIO ports IDs.
Definition at line
479
of file
em_gpio.h
.
Function Documentation
void GPIO_DbgLocationSet | ( | unsigned int |
location
|
) |
Sets the pin location of the debug pins (Serial Wire interface).
- Note
- Changing the pins used for debugging uncontrolled, may result in a lockout.
- Parameters
-
[in] location
The debug pin location to use (0-3).
Definition at line
79
of file
em_gpio.c
.
Referenced by DBG_SWOEnable() .
__STATIC_INLINE void GPIO_DbgSWDClkEnable | ( | bool |
enable
|
) |
Enable/disable serial wire clock pin.
- Note
- Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).
- Parameters
-
[in] enable
- false - disable serial wire clock.
- true - enable serial wire clock (default after reset).
Definition at line
623
of file
em_gpio.h
.
References BUS_RegBitWrite() .
__STATIC_INLINE void GPIO_DbgSWDIOEnable | ( | bool |
enable
|
) |
Enable/disable serial wire data I/O pin.
- Note
- Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).
- Parameters
-
[in] enable
- false - disable serial wire data pin.
- true - enable serial wire data pin (default after reset).
Definition at line
648
of file
em_gpio.h
.
References BUS_RegBitWrite() .
__STATIC_INLINE void GPIO_DbgSWOEnable | ( | bool |
enable
|
) |
Enable/Disable serial wire output pin.
- Note
- Enabling this pin is not sufficient to fully enable serial wire output, which is also dependent on issues outside the GPIO module. Refer to DBG_SWOEnable() .
- Parameters
-
[in] enable
- false - disable serial wire viewer pin (default after reset).
- true - enable serial wire viewer pin.
Definition at line
676
of file
em_gpio.h
.
References BUS_RegBitWrite() .
Referenced by DBG_SWOEnable() .
__STATIC_INLINE void GPIO_EM4DisablePinWakeup | ( | uint32_t |
pinmask
|
) |
Disable GPIO pin wake-up from EM4.
- Parameters
-
[in] pinmask
Bit mask containing the bitwise logic OR of which GPIO pin(s) to disable. Refer to Reference Manuals for pinmask to GPIO port/pin mapping.
Definition at line
707
of file
em_gpio.h
.
void GPIO_EM4EnablePinWakeup | ( | uint32_t |
pinmask,
|
uint32_t |
polaritymask
|
||
) |
Enable GPIO pin wake-up from EM4. When the function exits, EM4 mode can be safely entered.
- Note
- It is assumed that the GPIO pin modes are set correctly. Valid modes are gpioModeInput and gpioModeInputPull .
- Parameters
-
[in] pinmask
A bitmask containing the bitwise logic OR of which GPIO pin(s) to enable. See Reference Manuals for a pinmask to the GPIO port/pin mapping. [in] polaritymask
A bitmask containing the bitwise logic OR of GPIO pin(s) wake-up polarity. See Reference Manuals for pinmask-to-GPIO port/pin mapping.
Definition at line
356
of file
em_gpio.c
.
References GPIO_EM4SetPinRetention() , and GPIO_IntClear() .
Referenced by UTIL_shutdown() .
__STATIC_INLINE uint32_t GPIO_EM4GetPinWakeupCause | ( | void |
|
) |
Check which GPIO pin(s) that caused a wake-up from EM4.
- Returns
- Bit mask containing the bitwise logic OR of which GPIO pin(s) caused the wake-up. Refer to Reference Manuals for pinmask to GPIO port/pin mapping.
Definition at line
728
of file
em_gpio.h
.
__STATIC_INLINE void GPIO_EM4SetPinRetention | ( | bool |
enable
|
) |
Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.
- Note
- On series 0 devices EM4 gpio retention can either be turned on or off. On series 1 devices there are three EM4 GPIO retention modes available. These modes are "Disabled", "EM4EXIT" and "SWUNLATCH". Use the EMU_EM4Init() to configure the GPIO retention mode on a series 1 device.
The behavior of this function depends on the configured GPIO retention mode. If the GPIO retention mode is configured to be "SWUNLATCH" then this function will not change anything. If the retention mode is anything else then this function will set the GPIO retention mode to "EM4EXIT" when the enable argument is true, and "Disabled" when false.
- Parameters
-
[in] enable
- true - enable EM4 pin retention.
- false - disable EM4 pin retention.
Definition at line
760
of file
em_gpio.h
.
References BUS_RegBitWrite() .
Referenced by GPIO_EM4EnablePinWakeup() .
void GPIO_ExtIntConfig | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin,
|
||
unsigned int |
intNo,
|
||
bool |
risingEdge,
|
||
bool |
fallingEdge,
|
||
bool |
enable
|
||
) |
Configure the GPIO external pin interrupt.
It is recommended to disable interrupts before configuring the GPIO pin interrupt. See GPIO_IntDisable() for more information.
The GPIO interrupt handler must be in place before enabling the interrupt.
Notice that any pending interrupt for the selected interrupt is cleared by this function.
- Note
-
On series 0 devices, the pin number parameter is not used. The pin number used on these devices is hardwired to the interrupt with the same number.
On series 1 devices, the pin number can be selected freely within a group. Interrupt numbers are divided into 4 groups (intNo / 4) and valid pin number within the interrupt groups are: 0: pins 0-3 (interrupt number 0-3) 1: pins 4-7 (interrupt number 4-7) 2: pins 8-11 (interrupt number 8-11) 3: pins 12-15 (interrupt number 12-15)
- Parameters
-
[in] port
The port to associate with the pin
.[in] pin
The pin number on the port. [in] intNo
The interrupt number to trigger. [in] risingEdge
Set to true if the interrupt will be enabled on the rising edge. Otherwise, false. [in] fallingEdge
Set to true if the interrupt will be enabled on the falling edge. Otherwise, false. [in] enable
Set to true if the interrupt will be enabled after the configuration is complete. False to leave disabled. See GPIO_IntDisable() and GPIO_IntEnable() .
Definition at line
182
of file
em_gpio.c
.
References BUS_RegBitWrite() , BUS_RegMaskedWrite() , and GPIO_IntClear() .
Referenced by BOARD_alsEnableIRQ() , BOARD_envSensEnableIRQ() , BOARD_gasSensorEnableIRQ() , BOARD_hallSensorEnableIRQ() , BOARD_imuEnableIRQ() , BOARD_pushButtonEnableIRQ() , and GPIO_IntConfig() .
__STATIC_INLINE void GPIO_InputSenseSet | ( | uint32_t |
val,
|
uint32_t |
mask
|
||
) |
Enable/disable input sensing.
Disabling input sensing if not used, can save some energy consumption.
- Parameters
-
[in] val
Bitwise logic OR of one or more of: - GPIO_INSENSE_INT - interrupt input sensing.
- GPIO_INSENSE_PRS - peripheral reflex system input sensing.
[in] mask
Mask containing bitwise logic OR of bits similar as for val
used to indicate which input sense options to disable/enable.
Definition at line
806
of file
em_gpio.h
.
Referenced by ezradio_hal_GpioInit() .
__STATIC_INLINE void GPIO_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending GPIO interrupts.
- Parameters
-
[in] flags
Bitwise logic OR of GPIO interrupt sources to clear.
Definition at line
823
of file
em_gpio.h
.
Referenced by BOARD_alsClearIRQ() , BOARD_gasSensorClearIRQ() , BOARD_hallSensorClearIRQ() , BOARD_imuClearIRQ() , BOARD_picGetFwRevision() , BOARD_pushButton0ClearIRQ() , BOARD_pushButton1ClearIRQ() , GPIO_EM4EnablePinWakeup() , GPIO_ExtIntConfig() , and GPIOINT_CallbackRegister() .
__STATIC_INLINE void GPIO_IntConfig | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin,
|
||
bool |
risingEdge,
|
||
bool |
fallingEdge,
|
||
bool |
enable
|
||
) |
Configure GPIO interrupt.
If reconfiguring a GPIO interrupt that is already enabled, it is generally recommended to disable it first, see GPIO_Disable().
The actual GPIO interrupt handler must be in place before enabling the interrupt.
Notice that any pending interrupt for the selected pin is cleared by this function.
-
Deprecated:
- Deprecated function. New code should use GPIO_ExtIntConfig() .
- Note
- A certain pin number can only be associated with one port; i.e., if GPIO interrupt 1 is assigned to port A/pin 1, then it is not possible to use pin 1 from any other ports for interrupts. Refer to the reference manual. On devices which implement GPIO_EXTIPINSEL registers a more flexible approach is possible, refer to GPIO_ExtIntConfig() .
- Parameters
-
[in] port
The port to associate with pin
.[in] pin
The pin number on the port ( == GPIO EXTI interrupt number). [in] risingEdge
Set to true if interrupts will be enabled on rising edge, otherwise false. [in] fallingEdge
Set to true if interrupts will be enabled on falling edge, otherwise false. [in] enable
Set to true if interrupt will be enabled after configuration completed, false to leave disabled. See GPIO_IntDisable() and GPIO_IntEnable() .
Definition at line
1296
of file
em_gpio.h
.
References GPIO_ExtIntConfig() .
Referenced by BOARD_init() , BOARD_pushButtonEnableIRQ() , and ezradio_hal_GpioInit() .
__STATIC_INLINE void GPIO_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more GPIO interrupts.
- Parameters
-
[in] flags
GPIO interrupt sources to disable.
Definition at line
839
of file
em_gpio.h
.
Referenced by BOARD_picGetFwRevision() , and DisableSi114xInterrupt() .
__STATIC_INLINE void GPIO_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more GPIO interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using GPIO_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flags
GPIO interrupt sources to enable.
Definition at line
856
of file
em_gpio.h
.
Referenced by BOARD_picGetFwRevision() , and EnableSi114xInterrupt() .
__STATIC_INLINE uint32_t GPIO_IntGet | ( | void |
|
) |
Get pending GPIO interrupts.
- Returns
- GPIO interrupt sources pending.
Definition at line
868
of file
em_gpio.h
.
__STATIC_INLINE uint32_t GPIO_IntGetEnabled | ( | void |
|
) |
Get enabled and pending GPIO interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled GPIO interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in GPIO_IEN register and
- the OR combination of valid interrupt flags in GPIO_IF register.
Definition at line
888
of file
em_gpio.h
.
Referenced by GPIOINT_CallbackRegister() .
__STATIC_INLINE void GPIO_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending GPIO interrupts from SW.
- Parameters
-
[in] flags
GPIO interrupt sources to set to pending.
Definition at line
907
of file
em_gpio.h
.
Referenced by EnableSi114xInterrupt() .
__STATIC_INLINE unsigned int GPIO_PinInGet | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin
|
||
) |
Read the pad value for a single pin in a GPIO port.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin number to read.
- Returns
- The pin value, 0 or 1.
Definition at line
938
of file
em_gpio.h
.
References BUS_RegBitRead() .
Referenced by ADC0_IRQHandler() , BSP_McuBoard_UsbVbusOcFlagGet() , EnableSi114xInterrupt() , ezradio_hal_NirqLevel() , and TOUCH_IsBusy() .
GPIO_Mode_TypeDef GPIO_PinModeGet | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin
|
||
) |
Get the mode for a GPIO pin.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin number in the port.
- Returns
- The pin mode.
Definition at line
327
of file
em_gpio.c
.
void GPIO_PinModeSet | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin,
|
||
GPIO_Mode_TypeDef |
mode,
|
||
unsigned int |
out
|
||
) |
Set the mode for a GPIO pin.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin number in the port. [in] mode
The desired pin mode. [in] out
A value to set for the pin in the DOUT register. The DOUT setting is important for some input mode configurations to determine the pull-up/down direction.
Definition at line
278
of file
em_gpio.c
.
References GPIO_PinOutClear() , GPIO_PinOutSet() , and gpioModeDisabled .
Referenced by ADC0_IRQHandler() , BOARD_envSensEnable() , BOARD_flashDeepPowerDown() , BOARD_gasSensorEnable() , BOARD_hallSensorEnable() , BOARD_init() , BSP_BccPinsEnable() , BSP_BusControlModeSet() , BSP_EbiInit() , BSP_initBoard() , BSP_McuBoard_DeInit() , BSP_McuBoard_Init() , BSP_McuBoard_UsbVbusPowerEnable() , CAPLESENSE_setupGPIO() , CMU_ClkOutPinConfig() , DBG_SWOEnable() , ezradio_hal_GpioInit() , gpioInit() , I2CSPM_Init() , ICM20648_spiInit() , initGpio() , KSZ8851SNL_SPI_Init() , MIC_deInit() , MIC_init() , MICROSD_Deinit() , MICROSD_Init() , MSDD_Init() , RETARGET_SerialEnableFlowControl() , RETARGET_SerialInit() , sl_efp_init() , SPI_TFT_Init() , TFT_DirectGPIOConfig() , and UTIL_shutdown() .
__STATIC_INLINE void GPIO_PinOutClear | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin
|
||
) |
Set a single pin in GPIO data out port register to 0.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to set.
Definition at line
986
of file
em_gpio.h
.
References BUS_RegMaskedClear() .
Referenced by
BOARD_envSensEnable()
,
BOARD_flashDeepPowerDown()
,
BOARD_gasSensorEnable()
,
BOARD_gasSensorWake()
,
BOARD_hallSensorEnable()
,
BOARD_imuEnable()
,
BOARD_ledSet()
,
BOARD_micEnable()
,
BOARD_picGetFwRevision()
,
BOARD_rgbledEnable()
,
BOARD_rgbledPowerEnable()
,
BSP_McuBoard_UsbStatusLedEnable()
,
CAPT_enable()
,
ezradio_hal_ClearNsel()
,
ezradio_hal_DeassertShutdown()
,
GPIO_PinModeSet()
,
I2CSPM_Init()
,
KSZ8851SNL_SPI_SetChipSelect()
,
sl_efp_enter_em2()
, and
SPI_TFT_WriteRegister()
.
__STATIC_INLINE unsigned int GPIO_PinOutGet | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin
|
||
) |
Get current setting for a pin in a GPIO port data out register.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to get setting for.
- Returns
- The DOUT setting for the requested pin, 0 or 1.
Definition at line
1011
of file
em_gpio.h
.
References BUS_RegBitRead() .
__STATIC_INLINE void GPIO_PinOutSet | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin
|
||
) |
Set a single pin in GPIO data out register to 1.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to set.
Definition at line
1033
of file
em_gpio.h
.
References BUS_RegMaskedSet() .
Referenced by
BOARD_envSensEnable()
,
BOARD_flashDeepPowerDown()
,
BOARD_gasSensorEnable()
,
BOARD_gasSensorWake()
,
BOARD_hallSensorEnable()
,
BOARD_imuEnable()
,
BOARD_ledSet()
,
BOARD_micEnable()
,
BOARD_picGetFwRevision()
,
BOARD_rgbledEnable()
,
BOARD_rgbledPowerEnable()
,
BSP_McuBoard_UsbStatusLedEnable()
,
CAPT_enable()
,
ezradio_hal_AssertShutdown()
,
ezradio_hal_SetNsel()
,
GPIO_PinModeSet()
,
I2CSPM_Init()
,
initEbiCommon()
,
KSZ8851SNL_SPI_SetChipSelect()
,
sl_efp_enter_em0()
, and
SPI_TFT_WriteRegister()
.
__STATIC_INLINE void GPIO_PinOutToggle | ( | GPIO_Port_TypeDef |
port,
|
unsigned int |
pin
|
||
) |
Toggle a single pin in GPIO port data out register.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to toggle.
Definition at line
1060
of file
em_gpio.h
.
__STATIC_INLINE uint32_t GPIO_PortInGet | ( | GPIO_Port_TypeDef |
port
|
) |
Read the pad values for GPIO port.
- Parameters
-
[in] port
The GPIO port to access.
Definition at line
1080
of file
em_gpio.h
.
Referenced by BOARD_pushButtonGetState() .
__STATIC_INLINE void GPIO_PortOutClear | ( | GPIO_Port_TypeDef |
port,
|
uint32_t |
pins
|
||
) |
Set bits in DOUT register for a port to 0.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pins
Bit mask for bits to clear in DOUT register.
Definition at line
1102
of file
em_gpio.h
.
References BUS_RegMaskedClear() .
__STATIC_INLINE uint32_t GPIO_PortOutGet | ( | GPIO_Port_TypeDef |
port
|
) |
Get current setting for a GPIO port data out register.
- Parameters
-
[in] port
The GPIO port to access.
- Returns
- The data out setting for the requested port.
Definition at line
1124
of file
em_gpio.h
.
__STATIC_INLINE void GPIO_PortOutSet | ( | GPIO_Port_TypeDef |
port,
|
uint32_t |
pins
|
||
) |
Set bits GPIO data out register to 1.
- Note
- In order for the setting to take effect on the respective output pads, the pins must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pins
Bit mask for bits to set to 1 in DOUT register.
Definition at line
1146
of file
em_gpio.h
.
References BUS_RegMaskedSet() .
__STATIC_INLINE void GPIO_PortOutSetVal | ( | GPIO_Port_TypeDef |
port,
|
uint32_t |
val,
|
||
uint32_t |
mask
|
||
) |
Set GPIO port data out register.
- Note
- In order for the setting to take effect on the respective output pads, the pins must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] val
Value to write to port data out register. [in] mask
Mask indicating which bits to modify.
Definition at line
1176
of file
em_gpio.h
.
__STATIC_INLINE void GPIO_PortOutToggle | ( | GPIO_Port_TypeDef |
port,
|
uint32_t |
pins
|
||
) |
Toggle pins in GPIO port data out register.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pins
Bit mask with pins to toggle.
Definition at line
1200
of file
em_gpio.h
.
__STATIC_INLINE void GPIO_SlewrateSet | ( | GPIO_Port_TypeDef |
port,
|
uint32_t |
slewrate,
|
||
uint32_t |
slewrateAlt
|
||
) |
Set slewrate for pins on a GPIO port.
- Parameters
-
[in] port
The GPIO port to configure. [in] slewrate
The slewrate to configure for pins on this GPIO port. [in] slewrateAlt
The slewrate to configure for pins using alternate modes on this GPIO port.
Definition at line
1224
of file
em_gpio.h
.