IADC_ScanTableEntry_t Struct Reference

IADC scan table entry structure

Definition at line 765 of file em_iadc.h .

#include < em_iadc.h >

Data Fields

bool compare
uint8_t configId
bool includeInScan
IADC_NegInput_t negInput
IADC_PosInput_t posInput

Field Documentation

bool IADC_ScanTableEntry_t::compare

Perform digital window comparison on the result from this entry.

Definition at line 769 of file em_iadc.h .

Referenced by IADC_initScan() , and IADC_updateScanEntry() .

uint8_t IADC_ScanTableEntry_t::configId

Configuration id.

Definition at line 768 of file em_iadc.h .

Referenced by IADC_initScan() , and IADC_updateScanEntry() .

bool IADC_ScanTableEntry_t::includeInScan

Include this scan table entry in scan operation.

Definition at line 770 of file em_iadc.h .

Referenced by IADC_initScan() , and IADC_updateScanEntry() .

IADC_NegInput_t IADC_ScanTableEntry_t::negInput

Port/pin input for the negative side of the ADC.

Definition at line 766 of file em_iadc.h .

Referenced by IADC_initScan() , and IADC_updateScanEntry() .

IADC_PosInput_t IADC_ScanTableEntry_t::posInput

Port/pin input for the positive side of the ADC.

Definition at line 767 of file em_iadc.h .

Referenced by IADC_initScan() , and IADC_updateScanEntry() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_iadc.h