IADC_Config_t Struct Reference

IADC config structure

Definition at line 661 of file em_iadc.h .

#include < em_iadc.h >

Data Fields

uint8_t adcClkPrescale
IADC_CfgAdcMode_t adcMode
IADC_CfgAnalogGain_t analogGain
IADC_CfgOsrHighSpeed_t osrHighSpeed
IADC_CfgReference_t reference
IADC_CfgTwosComp_t twosComplement
uint32_t vRef

Field Documentation

uint8_t IADC_Config_t::adcClkPrescale

ADC_CLK divider (prescale+1).

Definition at line 667 of file em_iadc.h .

Referenced by IADC_init() .

IADC_CfgAdcMode_t IADC_Config_t::adcMode

IADC mode; Normal, High speed or High Accuracy.

Definition at line 662 of file em_iadc.h .

Referenced by IADC_init() .

IADC_CfgAnalogGain_t IADC_Config_t::analogGain

Analog gain.

Definition at line 664 of file em_iadc.h .

Referenced by IADC_init() .

IADC_CfgOsrHighSpeed_t IADC_Config_t::osrHighSpeed

Over sampling ratio for High Speed and Normal modes.

Definition at line 663 of file em_iadc.h .

Referenced by IADC_init() .

IADC_CfgReference_t IADC_Config_t::reference

Reference selection.

Definition at line 665 of file em_iadc.h .

Referenced by IADC_init() .

IADC_CfgTwosComp_t IADC_Config_t::twosComplement

Two's complement reporting.

Definition at line 666 of file em_iadc.h .

Referenced by IADC_init() .

uint32_t IADC_Config_t::vRef

Vref magnitude expressed in millivolts.

Definition at line 668 of file em_iadc.h .

Referenced by IADC_init() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_iadc.h