Detailed Description

USB HID keyboard scan codes.

Functions

char USB_HidScancodeToAscii (uint8_t scancode)
Converts the keyboard scancode to ASCII.

Variables

static const uint8_t Scancode2Ascii []
Table of keyboard scancode to ASCII mappings. Refer to the "HID Usage Tables" standard document from www.usb.org, section 10 "Keyboard/Keypad Page (0x07)".

Function Documentation

char USB_HidScancodeToAscii ( uint8_t scancode )

Converts the keyboard scancode to ASCII.

Parameters
[in] scancode Scancode you want to convert.
Returns
Scancode2Ascii .

Definition at line 58 of file usbkbdscancodes.c .

References Scancode2Ascii .