Capsense initialization structure.
Definition at line 605
of file em_acmp.h
.
#include <
em_acmp.h
>
Data Fields | |
uint32_t | biasProg |
bool | enable |
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
ACMP_CapsenseResistor_TypeDef | resistor |
uint32_t | vrefDiv |
Field Documentation
uint32_t ACMP_CapsenseInit_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line 620
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit(), and CAPLESENSE_setupACMP().
bool ACMP_CapsenseInit_TypeDef::enable |
If true, ACMP is enabled after configuration.
Definition at line 679
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel |
ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor |
A resistor used in the capacative sensing circuit. For values see the device data sheet.
Definition at line 642
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
uint32_t ACMP_CapsenseInit_TypeDef::vrefDiv |
VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
Definition at line 653
of file em_acmp.h
.
Referenced by ACMP_CapsenseInit().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_acmp.h